Good morning,
I am planning to control the switch AGG1611 with a digital output 5 V from Arduino. I saw that the input is 3V-compatible. Is it possible to use directly the Arduino 5V output or I need to reduce it?
Thank you,
Alessandro
ADG1611
Production
The ADG1611 / ADG1612 / ADG1613 contain four independent single-pole/single-throw (SPST) switches. The ADG1611 and ADG1612 differ only in that the digital...
Datasheet
ADG1611 on Analog.com
Good morning,
I am planning to control the switch AGG1611 with a digital output 5 V from Arduino. I saw that the input is 3V-compatible. Is it possible to use directly the Arduino 5V output or I need to reduce it?
Thank you,
Alessandro
Hello,
It is possible to use 5V to control the ADG1611 providing the Vdd is at least 5 V also. the digital control voltage must not exceed the supply.
Regards,
David