ADG901 with 3.3 V Supply

Has anyone tried using the ADG901 with a 3.3 V supply and signal levels?

The maximum VDD to ground rating is 4 V. I just want to use this for some prototyping and just power it directly from the microcontroller board I'm using.

  • 0
    •  Analog Employees 
    on Dec 5, 2019 10:10 AM

    Hi David,

    ADG901 is operation from VDD = 1.65V to 2.75V as displayed in specification table. Operating the switch above the specification voltage may impact the reliability of the switch. The maximum voltage to ground rating specified in the AMR table is once off stress rating only. I will not recommend you to operate ADG901 above 2.75V.

    Thanks

    Naveen