Hi, I am trying to switch out a bunch of signals so I used the ADG726. Unfortunately, the signals need over 2.5V but also below 0V so I couldn't go with either the 0V to 5V nor the -2.5V to 2.5V recommendations in the datasheet. In order to achieve the switching requirements of both sides, I connected the VDD pins to +4V and the VSS to -1.42V. Do you think this is an acceptable use case for this IC? Also do you foresee any reliability issues due to connecting it in such a manner? Thanks!