Post Go back to editing

About characteristic change by temperature change of ADG1434

Thread Summary

The user inquired about the ADG1434's pin capacitance (CD, CS) changes with temperature and input voltage. The support engineer stated that there should not be significant changes in capacitance or bandwidth with temperature, and capacitance changes slightly with input voltage. The ADG1234 was suggested as an alternative with lower capacitance and higher bandwidth, including plots of capacitance vs input voltage in its datasheet.
AI Generated Content

Hello,

Could you let me know the following information about ADG1434?

1. Does the pin capacitance (CD,CS) change significantly with changes in temperature or input voltage?

2. Fig. 22 of the data sheet P12 is a figure at 25 ° C, does the characteristic change significantly under the conditions of 15 ° C and 35 ° C?

Regards,
Tatsu