Hello. I want use muliplexer adg1633 in package 3x3 16-pin LFCSP. But i have only +3.3V, +2.5V and -2.5V power supplyes(+-2.5V for AD8616 with max 5.5V supply and cant do +-3.3V) . And have no -3.3v.
In datasheet Vss must be 0V in unipolar mode or -3.3...-8V in bipolar mode.
Signal amplitude in this multiplexers will be <1.5V.
Can i use bipolar supplyes Vdd=3.3V and Vss=2.5V?
Thanks.
HI,
The ADG1633 should function with Vdd = 3.3V and Vss= 2.5 V, however we do not guarantee any parameter performance at these supplies.
Have you looked at the ADG733 or the ADG786, this is fully specified at +/-2.5 V supply.
This might be a better option.
Regards,
David