AD8010
Production
The AD8010 is a low power, high current amplifier capable of
delivering a minimum load drive of 175 mA. Signal performance
such as 0.02% and 0.03° differential...
Datasheet
AD8010 on Analog.com
AD8180
Production
The AD8180 (single) and AD8182 (dual) are high speed 2-to-1 multiplexers. They offer -3 dB signal bandwidth greater than 780 MHz along with slew rate...
Datasheet
AD8180 on Analog.com
HI,
we are implementing 2 to 1 multiplexing circuit using AD8180.
Application1: Toggle between 0V and 1.3V using SELECT Pin ( i.e, 0/5V TTL).
Application2: Toggle between -0.6 V and -5V using SELECT Pin ( i.e, 0/5V TTL).
In both cases we are getting zero output even with Enable pin Low (GND) and Select pin toggle between 0V and 5V.
By suspecting IC failure i have replaced with new ones.but facing same problem.
please suggest a solution.
Regards
GPR
Hi,
Your schematic looks fine. May I see your current setup? How are you evaluating the part? Have you checked your connections whether there is cold solders?
Regards,
Goz