Post Go back to editing

ADG701 Leakage Current

Thread Summary

The user inquires about the worst-case leakage current of the ADG701 over the operational temperature range (-40 to 85°C). The final answer suggests using the ADG701L, which has leakage specified across the full temperature range, ensuring it remains below 100nA.
AI Generated Content

Hello, 

We're considering using the ADG701 in an application that requires a very low leakage current (switching a very small current source to ground). 

The datasheet specifies 10pA typical at 25 degrees celsius, but no figure is quoted for the operational range (-40-85). We'd like to know the worst case leakage figure for this part -- is this available? 

If there are any other functionally equivalent alternatives where this can be guaranteed to be low (< 100nA) over the operational range, then we would be open to consider.  

Thank you for your assistance