Post Go back to editing

ADG5248F HBM ESD

Thread Summary

The user inquired about the HBM ESD rating of the ADG5248F, which is confirmed to be 3.5kV. The datasheet's Figure 52 indicates that the Sx pin can withstand ESD up to 3.5kV, and the diodes between D/Dx pins and POSV or NEGV can handle ±55V. For surge voltages over 3.5kV, additional TVS or protection devices are recommended. The ADG1408 has a 2kV HBM ESD rating.
AI Generated Content

Hi

Regarding ADI web, ADG5248F's HBM ESD is 3.5kV on the link. But we couldn't see the spec on the datasheet. Would 3.5kV be correct spec ?

https://www.analog.com/en/products/switches-multiplexers/fault-protected-switches-multiplexers.html

Regards,

Hiroyuki

  • HI Hiroyuki,

    Yes 3.5kV is correct for the ADG5248F.

    Regards,

    David

  • Dear David

    Thank you very much for your support. This question and below link one are given by the same customer.

    https://ez.analog.com/switches_multiplexers/f/q-a/107891/adg5408-power-off-protection

    Actually ADG5248F is connected to the user interface then he has to take care of ESD.

    My understand what Figure 52 in ADG5248F datasheet means is that ESD protection on Sx pin withstand ESD up to 3.5kV and the diode located between D/Dx pin and POSV or NEGV withstand up to +-55V. Would it be correct ?

    If a surge voltage over 3.5kV would hit on Sx or D/Dx, it would be broken ? Then TVS or any protection device would be needed to connect with the pins ?

    On the other hand ADG1408 is lower Ron. How much its capability of ESD protection ?

    Regards,

    Hiroyuki    

  • Dear David

    Sorry for my pushing. Could you give me the answer ?

    Regards,

    Hiroyuki

  • Hi Hiroyuki,

    Apologies for they delayed response. I was out of the office last week.

    "My understand what Figure 52 in ADG5248F datasheet means is that ESD protection on Sx pin withstand ESD up to 3.5kV and the diode located between D/Dx pin and POSV or NEGV withstand up to +-55V. Would it be correct ?"

    This is correct however I would point out that this is HBM ESD.

    What ESD standard are you trying to protect against? If it is system level ESD you should take a look at our application note AN-1436.

    This application note details testing we have done with the ADG5412F and a discrete TVS and Resistor to achieve ESD protection to the IEC61000-4-2 standard.

    However I have to note that the ADG5248F was not tested and would likely need larger resistance after the TVCS butt the same principle should apply.

    The ADG1408 is rated for2kV HBM ESD. 

    Thanks

    David