Post Go back to editing

ADG1213 max digital IN voltage at power down

Thread Summary

The user inquires about the safe voltage to apply to the digital in selector pins of the ADG1213 when it is not powered up. The support engineer confirms the maximum safe voltage is 0.3 V due to protection diodes. The ADG5413F is suggested as an alternative with power-off protection, but the user plans to use a buffer amp on the same power supply to protect the ADG1213.
AI Generated Content

Hi,
what voltage is save to apply to the digital in selector pins on the ADG1213 when it is not powered up?
The data sheet references max IN voltage to VDD, i.e. for power down this would give max V = 0 + 0.3 = 0.3V?
While the data sheet mentions protection diodes (to not exceed 30mA), I'm not sure when these will kick in.
Using an ADG1234 in the past, I never noticed an issue applying V_hi=3V @IN when powered down, but in a current layout using the ADG1213 it looks like it causes issues.

Cheers

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.