Post Go back to editing

ADG1438 and ADG1439 switches input voltages in single-supply mode

Thread Summary

The user inquires about the operational voltage range of a switch in single-supply mode and confirms if Vss and GND can be connected together. The support engineer clarifies that the device operates safely within +5 V to +16.5 V for single supply, and suggests the ADG5408 for higher voltage needs. The user requires a higher channel count and random access, leading to a recommendation of the ADGS5414, an SPI-controlled 8 x SPST switch with a VDD up to +40V, and a request for a higher channel count switch, ideally 16 x 2, to reduce the number of ICs needed.
AI Generated Content

Based on the information from the data sheet I assume these switches can be powered in single-supply mode with Vdd up to +25V max. (Vss and GND connected together) with safe input voltages within 0V to Vdd range with any internal switches configuration. At the same time VL (logic supply) can be anywhere in the range from 2.7 V to 5.5 V. 

Please confirm these assumptions are correct.

Thanks!

  • Hi,

    The +25 V Max you are referring to comes from the Absolute max ratings table. This is a stress rating that indicates the device will not suffer damage below this voltage. However it does not indicate functionality.

    The device is guaranteed to be operational with in the range +/-4.5 V to +/-16.5 V for dual supply and +5 V to +16.5 V for single supply. These are outlined in the datasheet in table 2 for dual supply and table 3 for single supply.

    If you are looking for higher voltage supply our ADG5408 device may be of interest. This has a single supply range of 9 V to 44 V.

    Would this work for you?

    Regards,

    David

  • Thank you for your reply David,

    ADG5408 has parallel interface and only one switch can be engaged at a time. I need to randomly access to 200+ channels with voltages up to +18V and as long as 18V is OK I'm fine. Potentially I can connect Vss to the GND and level shift SPI but better not to.

    I would appreciate your input David,

    Thanks,

    Nikolai

  • Hi Nikolai,

    A product like the ADGS5414 could an option for you here. It is a SPI controlled 8 x SPST switch which can be powered with a VDD upto +40V.

    The break before make switching of the device enables it to be configured as a mux by external wiring on the PCB and you would be able to select all channels if you like. The following Application Note details the break before make feature in the ADGS5414.

    https://www.analog.com/media/en/technical-documentation/application-notes/an-1485.pdf

    Regards,

    Stephen

  • Thank you Stephen,

    It should work. Are there any chance you have higher count switches (preferably N x 2)? I need randomly connect 204 channels either to GND or test voltage and it will require 52 ICs

    Something like MAX14661 chip (16 x 2), but with up to +18V input range. In this case only 13 ICs would be enough. Huge space difference.

    Nikolai

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.