Post Go back to editing

SPICE model of ADG2188

Hi,

I am looking for to simulate ADG2188 switch in my circuit which I am using to switch multiple SPI interfaces. Please provide the SPICE model of ADG2188.

Thanks,

Saril



update the correct tag adg2188
[edited by: sarilkaiprath at 5:35 PM (GMT -4) on 9 Oct 2018]
Parents Reply
  • Hi Saril,

    Apologies, an HSPICE model is also not available.

    With regards to the propagation delay of x to y question, it should be same as Ton/Toff as this is measured after the 3-byte write (8-bit device address & two 8-data bits). Kindly see page 20 of the ADG2188 datasheet.

    Any changes to x and y channels will be read after all address and data bits are written.

    Let me know if this helps.

    Best Regards,

    May

Children