Post Go back to editing

ADG 1413 LTspice simulation

Thread Summary

The user encountered an issue where the ADG 1413 was outputting only about half the input voltage (4 V for a 10 V input) in a simulation. The final answer confirmed that the issue was addressed offline, without providing specific details. The accompanying answer acknowledged the query and indicated that someone was investigating the problem.
AI Generated Content

Hi,

he customer is considering using ADG 1413 and received questions about the simulation.

In the circuit diagram below, when using the ADG 1413, when inputting a 10 V signal, the output was only about 4 V.

Even if it is changed to other conditions, only about half the input voltage is output, but is the simulation suitable?

Best regards,

Yuya

Edit Notes

Add centense
[edited by: Yuya at 8:40 AM (GMT -4) on 2 Oct 2018]