According to the curve between the logic high level and power supply voltage in the MAX4733 datasheet, when V+ is 9V, VIH should be greater than 2.3V.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
According to the curve between the logic high level and power supply voltage in the MAX4733 datasheet, when V+ is 9V, VIH should be greater than 2.3V.