Are the LEDs ports also bidirectional like the other signals ports?
Answer:
Yes, the MAX4892E LED switches are analog switches that pass signals equally in either direction; they are not restricted to one direction only as users might believe based on the pin description table, page 5 in the datasheet. The On resistance is listed in the electrical characteristics table page 2, maximum 40 Ohms.
.