Article What kind of resolution does the MAX14983E support?

Given that the quality of the data channel being at its most optimal, the supported resolution of the MAX14983 is limited by its specified RGB max switching bandwidth at about 800MHz. If the product of Htotal x Vtotal x Framerate (which would be the pixel rate) is less than 800MHZ the MAX14983E the RGB switching bandwidth should not exceed 800MHz and therefore can be supported with the MAX14983.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.