Article MAX14756 NC On resistance when unpowered

Question: The MAX14756 is listed as normally closed (NC).  If the device is unpowered, will it pass signals and have its closed on-resistance through the A_ to B_ paths?

Answer: No, the NC designation just refers to how the device responds to control signals when powered. If the device is unpowered, it would not operate normally with a low on-resistance path between A_ and B_.   If signals are present at the A_ and B_ terminals while the device is not powered (VDD = 0V), ensure that the absolute maximum ratings are not exceeded (datasheet, page 2):

A_, B_ to VSS............................... -0.3V to (VDD + 2V) or 100mA (whichever occurs first)

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.