Article ADG412: Lower voltage supplies than specified

Question

Can switches and multiplexers be operated with logic power supplies less than
those specified in the data sheet, eg. with 3.3 volts.

Answer

Specifically the ADG412 is specified from 4.5 to 5.5V i.e. 5V +/-5%. If you go
outside this range then the device is not guaranteed to function reliably or to
specification.

Our ADG1212 is compatible with TTL levels (Vih = 2V minimum) and has no digital
supply pin - it is simply powered from the analog supply (+12V or +/-15V).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.