MAX3890: FAQ

  • Created
  • Updated
Was this helpful?
  • Reducing MAX3890 parallel clock frequency

    Q: The MAX3890 specifies acceptable input parallel clocks of 155.52MHz, 77.76MHz, 51.84MHz, and 38.88MHz. Is it possible to use the chip with other clock frequencies such as 96MHz? A: No other rates are…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.