ADG884: FAQ

  • Created
  • Updated
Was this helpful?
  • ADG884 Overvoltage

    Question Why does the ADG884 switch get stuck at a certain voltage when the input voltage exceeds the maximum ratings? Answer Under or overvoltage spikes can trigger parasitics in the part that cause…
  • ADG884: Bandwidth simulation

    Question I´m using the spice model of the ADG884. In the datasheet the -3dB Bandwidth is 18MHz. In the simulation the result is about 1.7GHz. Is the analog bandwidth of the signal chain not contained…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.