Article When supplied with -2.5V and+2.5V, can the ADG788 accept the same voltage swing at its logic control pins?

When supplied with ±2.5V dual supply rails, the ADG788 analog pins have the same VSS to VDD range, but the control pins or digital pins are referenced to GND so these have a range of -0.3V to VDD+0.3V. There are internal diodes on these pins to the supply lines hence the 0.3V clamping voltage. Current into these pins must not exceed 30mA.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.