Article ADG709: Life time

Question

Here is 2 questions about ADG709 :

(CMOS, 1.8V to 5.5V/+-2.5V, 3Ohm, Low Voltage, 4-/8-Channel Multiplexers)

1 - What is the typical expected life (nb. of switches) of MOS comutations for
a typical application ?

1 - What is the typical expected life (nb. of switches) of MOS comutations for
a 30mA maximal continuous current (hot switching) ?

Answer

We don't specify this parameter. We do however, run the device for a length of
time , say 168 hours or 1000 hours at a high temperature, be it 85 deg or 125
deg, depending on the specification of the device. From this we calculate the
expected lifetime of the device.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.