ADG506: FAQ

  • Created
Was this helpful?
  • ADG506: Overvoltage on the input

    Q Problem with given configuration : During above operating mode, the multiplexer input (protection circuit) limits the input voltage to » 720mV. The current drawn by the input during this phase is …
  • ADG506: Pin connection

    Q We have a design using two ADG506 multiplexers where the two output signals on pins 28 are connected together. When either device is selected we cannot obtain a signal from pin 28 as the other device…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.