ADG3304: FAQ

  • Created
  • Updated
Was this helpful?
  • ADG3304: Is this device compatible with I2C?

    Q I am using ADG3304 to buffer between a 3.3V processor and a 1.8V I2C peripheral. It works OK but it does not like the I2C state when momentarily no one is driving the data line. Is it suitable for…
  • ADG3304: used as I2C level shifter

    Q I want to interface an 5V I2C EEPROM with my 3.3V MCU by ADG3304 Can ADG3304 be suitable for this applicaton, the I2C SDA is input/output signal A I'm afraid we don't have a part that would be…
  • ADG3304_power up sequence

    Q I have contacted with the customer and he will do the test with normal 3.3V / 2.8V power supply tomorrow morning to see the result. If there is still some problem, I will visit them to check the detail…
  • ADG3304_protection method

    Q I checked the datasheet, this part can work with the same power supply on Vcca and Vccy, but some cautions should be noted: 1. the power supply issue on page 16 of its datasheet. 2. For not high speed…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.