AD8152 EVB: FAQ

  • Created
  • Updated
Was this helpful?
  • AD8152 EVB

    Q AD8152 EVB schematic A Please refer to the attached Attachments: AD8152EBSchematic.zip
  • AD8152: Connection of DC inputs

    Q I am running the AD8152 on VEE=0, VCC=+2.5V and would like to drive the inputs of the inputs, DC couple, from LVPECL with a common mode range of +1.5V to +2.3V. Can I connect VTTI to ground via a …
  • AD8152: used as a DVI switch

    Q Can you suggest whether AD8152 can be used in DVI application for the TMDS link switching? A We have not tested this, but everything should be good for the AD8152 to handle the TMDS signals for…
  • AD8152_switch HDMI signals

    Q I want to use AD8152 as a HDMI cross point switch. Can I use the HDMI signal. Also if it can be used, can I cascade several AD8152s to implement a larger matrix. A 1. Yes, the AD8152 can be uses…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.