I'm using the Transceiver Toolbox to target my own HDL model on the ZC706 + ADRV9375 platform, and I believe I've encountered a bug in the latest release (v23.2.2).
To verify basic functionality, I built the simplest example model, "testModel_Rx16Tx32_regs.slx", located in the `test` folder. This is the simple delay model provided by the Transceiver Toolbox project. Using MATLAB 2023b and Vivado 2022.2, the model compiles successfully without any errors.
However, when I copy the generated BOOT.bin file to the SD card and boot the platform, the system fails to operate correctly. I used the official device tree and uImage files directly from the 2022_R2 SD card.
The observed behavior is as follows:
- When connected via IIO Oscilloscope, the Rx RF bandwidth of the ADRV9375 is not displayed properly; it shows "<error>" instead of a valid value.
- I cannot load any profile to change the ADRV9375 configuration — it always reports "failed".
- No data is received from the board; IIO Oscilloscope cannot capture any samples once streaming starts.
Screenshots for these behaviors:



I'm confident that the issue originates from the generated FPGA image (BOOT.bin). When I replace it with the official BOOT.bin, the system immediately works as expected.
For further verification, I tested an older Transceiver Toolbox release (v23.2.1) using MATLAB 2023b and Vivado 2021.2. The same model works perfectly in that setup.
Therefore, I strongly suspect this issue is a bug introduced in Transceiver Toolbox v23.2.2.