KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
I have tried multiple ways to implement precise DOA estimation on The Phaser kit, one of them being the popular MUSIC algorithm. As the kit has two subarrays, it is possible to detect the precise DOA of only one object. The problem is that every time I run the script I get an estimated DOA around plus/minus 20 degrees even though the transmitter is placed at mechanical boresight or at some other angle.
Below attached is the code that I have created. Please suggest me on what changes should i make to properly implement the algorithm.
Also I read about phase mismatch between the two Rx channels of the PlutoSDR, could that cause problems??
import adi
from adi import ad9361
from adi.cn0566 import CN0566
import matplotlib.pyplot as plt
import numpy as np
from scipy import signal
from numpy.fft import fft, fftfreq, fftshift
import ADAR_pyadi_functions as ADAR
import helper_funcs
import SDR_functions as SDR
import aic
from doa_py import arrays, signals
from doa_py.algorithm import music
from doa_py.plot import plot_spatial_spectrum
#Key Parameters
sample_rate = 30e6
center_freq = 2.2e9
signal_freq = 100e4
rx_gain = 60
d = 0.056
c= 299792458
#%% Initial Setup
# Instantiate all the Devices
rpi_ip = "ip:phaser.local" # IP address of the Raspberry Pi
sdr_ip = "ip:192.168.2.1" # "192.168.2.1, or pluto.local" # IP address of the Transceiver Block
my_sdr = adi.ad9361(uri=sdr_ip)
my_phaser = adi.CN0566(uri=rpi_ip)
# Initialize both ADAR1000s, set gains to max, and all phases to 0
my_phaser.configure(device_mode="rx")
my_phaser.load_gain_cal()
my_phaser.load_phase_cal()
for i in range(0, 8):
my_phaser.set_chan_phase(i, 0)
gain_list = [127,127,127,127,127,127,127,127]
for i in range(0, len(gain_list)):
my_phaser.set_chan_gain(i, gain_list[i])
# Setup Raspberry Pi GPIO states
my_phaser._gpios.gpio_tx_sw = 0 # 0 = TX_OUT_2, 1 = TX_OUT_1
my_phaser._gpios.gpio_vctrl_1 = 1 # 1=Use onboard PLL/LO source (0=disable PLL and VCO, and set switch to use external LO input)
my_phaser._gpios.gpio_vctrl_2 = 1 # 1=Send LO to transmit circuitry (0=disable Tx path, and send LO to LO_OUT)
# Configure SDR Rx
my_sdr.sample_rate = int(sample_rate)
sample_rate = int(my_sdr.sample_rate)
my_sdr.rx_lo = int(center_freq)
my_sdr.rx_enabled_channels = [0, 1] # enable Rx1 and Rx2
my_sdr.gain_control_mode_chan0 = "manual" # manual or slow_attack
my_sdr.gain_control_mode_chan1 = "manual" # manual or slow_attack
my_sdr.rx_hardwaregain_chan0 = int(rx_gain) # must be between -3 and 70
my_sdr.rx_hardwaregain_chan1 = int(rx_gain) # must be between -3 and 70
my_sdr.rx_buffer_size = 2**12
my_sdr.rx_rf_bandwidth = int(2e6)
# Setup Raspberry Pi GPIO states
my_phaser._gpios.gpio_tx_sw = 0 # 0 = TX_OUT_2, 1 = TX_OUT_1
my_phaser._gpios.gpio_vctrl_1 = 1 # 1=Use onboard PLL/LO source (0=disable PLL and VCO, and set switch to use external LO input)
my_phaser._gpios.gpio_vctrl_2 = 1 # 1=Send LO to transmit circuitry (0=disable Tx path, and send LO to LO_OUT)
# Configure SDR Tx
my_sdr.tx_lo = int(center_freq)
my_sdr.tx_enabled_channels = [0, 1]
my_sdr.tx_cyclic_buffer = True # must set cyclic buffer to true for the tdd burst mode.
my_sdr.tx_hardwaregain_chan0 = -88 # must be between 0 and -88
my_sdr.tx_hardwaregain_chan1 = -0 # must be between 0 and -88
# Configure the ADF4159 Ramping PLL
output_freq = 12.725e9
my_phaser.frequency = int(output_freq / 4) # Output frequency divided by 4
my_phaser.ramp_mode = "disabled" # ramp_mode can be: "disabled", "continuous_sawtooth", "continuous_triangular", "single_sawtooth_burst", "single_ramp_burst"
my_phaser.enable = 0 # 0 = PLL enable. Write this last to update all the registers
# Intialize the ADAR1000 receive array
rx_array = adi.adar1000_array(
uri=rpi_ip,
chip_ids=["BEAM0", "BEAM1"], # these are the ADAR1000s' labels in the device tree
device_map=[[1], [2]],
element_map=[[1, 2, 3, 4, 5, 6, 7, 8]],
device_element_map={
1: [8,7,5,6], # i.e. channel2 of device1 (BEAM0), maps to element 8
2: [4,3,1,2],
},
)
for device in rx_array.devices.values():
ADAR.ADAR_init(device) # resets the ADAR1000
ADAR.ADAR_set_mode(device, "rx") # ADAR1000s on Phaser are receive only, so mode is always "rx"
# Create a sinewave waveform
fs = int(my_sdr.sample_rate)
N = int(my_sdr.rx_buffer_size)
fc = int(signal_freq / (fs / N)) * (fs / N)
ts = 1 / float(fs)
t = np.arange(0, N * ts, ts)
i = np.cos(2 * np.pi * t * fc) * 2 ** 14
q = np.sin(2 * np.pi * t * fc) * 2 ** 14
iq = 1 * (i + 1j * q)
# Send data
my_phaser.sdr = my_sdr
my_phaser.sdr._ctx.set_timeout(0)
my_phaser.sdr.tx([iq * 0.5, iq])
nSamples=my_phaser.sdr.rx_buffer_size
#%% MUSIC Algorithm
nSamples = my_phaser.sdr.rx_buffer_size
signal_mat=np.zeros((nSamples,2),dtype=complex)
data = my_phaser.sdr.rx()
signal_mat[:,0] = data[0]
signal_mat[:,1] = data[1]
plt.plot(data[0])
plt.plot(data[1])
print("\n\tsignal matrix\n")
print(signal_mat)
ula = arrays.UniformLinearArray(m=2, dd=0.015)
# Calculate the MUSIC spectrum
angle_grids = np.arange(-90, 90, 0.1)
spectrum = music(
received_data=signal_mat.T,
num_signal=1,
array=ula,
signal_fre=10.525e9,
angle_grids=angle_grids,
nSamples=nSamples,
unit="deg",
)
# Plot the spatial spectrum
plot_spatial_spectrum(
spectrum=spectrum,
ground_truth=np.array([0,]),
angle_grids=angle_grids,
num_signal=1,
)
#%%Destroy
my_phaser.sdr.tx_destroy_buffer()
Cristianmihaipopa1601 - Moved from Virtual Classroom for ADI University Program to Software Interface Tools. Post date updated from Tuesday, June 10, 2025 7:39 PM UTC to Wednesday, June 11, 2025 10:48 AM UTC to reflect the move.
Any phase mismatch between the two digital pluto receivers can be calibrated out. And this is done in the examples. But algorithm development is outside of the support we can offer on ADI's EngineerZone. I have found this to be a good resource though: pysdr.org/.../doa.html