Post Go back to editing

pyadi-iio with ADRV9025

Category: Software
Product Number: ADRV9026
Software Version: libiio-0.25, pyadi-iio-0.0.16

I have a ZCU102 with ADRV9025 libiio subsystem device loaded, and am trying to interface with the following API to set parameters on the RF transceiver. I was hoping to do this with pyadi-iio; however, I do not see ADRV9025 (or ADRV9026/ADRV9029) available as supported devices. I do see ADRV9009 as a supported device, and my understanding is that the ADRV9009 is the two-channel version of the four-channel ADRV9025. Can I use the adrv9009.py ADI API to begin interfacing with my subsystem, or would the names need to match? I was thinking of creating my own adrv9025.py based on the adrv9009.py, but wanted to ask to see if this device might already be in the works of being supported. 

Subsystem screenshot: