Post Go back to editing

ADRV9361-Z7035 not booting

Category: Hardware

I have the ADRV9361-Z7035 and FCM carrier straight out of the box. I copied the associated boot files including uimage to the boot directory, and I set all the switches to the correct configuration for booting from SD (all set to 1 for carrier SD card). D3 and D4 come on on the SOM and stay on. DS8 comes on on the carrier. No uart messages come out to the PC. Nothing comes up on the monitor connected via HDMI. I tried booting from the SoM and carrier. Nothing. I reimaged the SD card that came with the carrier board. Still nothing.