Post Go back to editing

using adrv9009zu11eg transmit signal with both TX channel at the same time on MATLAB

Category: Software
Software Version: matlab 2022b SD image 2022_r2

Hi,

I being using 9009zu11eg board on matlab for a while, I have tested using 2 Rx channels to receive at the same time, using ".enabledchannels[1,2]", I followed all the instruction on adi doc and it works.

But when it comes to the Tx end, it didn't work (I'm using the same properties “enabledchannels”). I want to send signal with multiple Tx channels, what should I do, or is there any properties than I didn't set properly.