Post Go back to editing

Installing FMCOMMS5 DOA estimation GNU Radio tool -- gr-doa

Category: Software

Hi all,

I want to do DOA estimation experiments with FMComms5 board with the help of GNU radio. I am trying to install the gr-doa tool found at -  https://github.com/tfcollins/gr-doa/tree/adi. However I am facing some problems:

cmake ..

-- Could NOT find PythonLibs (missing: PYTHON_LIBRARIES PYTHON_INCLUDE_DIRS) (Required is at least version "2")
-- Could NOT find PythonInterp (missing: PYTHON_EXECUTABLE) (Required is at least version "2")
CMake Error at cmake/Modules/GrPython.cmake:113 (file):
  file FILE([TO_CMAKE_PATH|TO_NATIVE_PATH] path result) must be called with
  exactly three arguments.
Call Stack (most recent call first):
  python/CMakeLists.txt:23 (include)


-- Could NOT find PythonInterp (missing: PYTHON_EXECUTABLE) (Required is at least version "2")
CMake Error at cmake/Modules/GrPython.cmake:113 (file):
  file FILE([TO_CMAKE_PATH|TO_NATIVE_PATH] path result) must be called with
  exactly three arguments.
Call Stack (most recent call first):
  apps/CMakeLists.txt:20 (include)


-- Configuring incomplete, errors occurred!

Hence, I specify the python libraries, include directories and executable to the cmake command, but the problem remains the same:

cmake -DPYTHON_LIBRARIES=/usr/include/python3.10 -DPYTHON_INCLUDE_DIRS=/usr/lib/x86_64-linux-gnu/libpython3.10.so -DPYTHON_EXECUTABLE=/usr/bin/python3 -Wno-dev ..

-- Could NOT find PythonLibs (missing: PYTHON_LIBRARIES PYTHON_INCLUDE_DIRS) (Required is at least version "2")
  File "<string>", line 3
    print sysconfig.get_python_lib(plat_specific=True, prefix='')
    ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
SyntaxError: Missing parentheses in call to 'print'. Did you mean print(...)?
CMake Error at cmake/Modules/GrPython.cmake:113 (file):
  file FILE([TO_CMAKE_PATH|TO_NATIVE_PATH] path result) must be called with
  exactly three arguments.
Call Stack (most recent call first):
  python/CMakeLists.txt:23 (include)


Traceback (most recent call last):
  File "<string>", line 2, in <module>
TypeError: Strings must be encoded before hashing
  File "<string>", line 3
    print sysconfig.get_python_lib(plat_specific=True, prefix='')
    ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
SyntaxError: Missing parentheses in call to 'print'. Did you mean print(...)?
CMake Error at cmake/Modules/GrPython.cmake:113 (file):
  file FILE([TO_CMAKE_PATH|TO_NATIVE_PATH] path result) must be called with
  exactly three arguments.
Call Stack (most recent call first):
  apps/CMakeLists.txt:20 (include)


Traceback (most recent call last):
  File "<string>", line 2, in <module>
TypeError: Strings must be encoded before hashing
CMake Error at cmake/Modules/GrPython.cmake:125 (add_custom_target):
  add_custom_target cannot create target "ALL" because another target with
  the same name already exists.  The existing target is a custom target
  created in source directory "/home/ennio/github/gr-doa/python".  See
  documentation for policy CMP0002 for more details.
Call Stack (most recent call first):
  cmake/Modules/GrPython.cmake:228 (GR_UNIQUE_TARGET)
  apps/CMakeLists.txt:22 (GR_PYTHON_INSTALL)


-- Configuring incomplete, errors occurred!

How can I fix this?

Thanks,

Ennio

Parents
  • That gr-doa build was based on GR 3.7 which requires python 2. You cannot simply change the pointed to python version and make things function in python 3.

    -Travis

  • Hi Travis,

    Thanks for your reply.

    Now I am running GR 3.7.14 and python 2.7.17. The code seems to build well, but I have problems when running the "make test" command.
    First, this is the output of cmake:

    -- The CXX compiler identification is GNU 7.5.0
    -- The C compiler identification is GNU 7.5.0
    -- Check for working CXX compiler: /usr/bin/c++
    -- Check for working CXX compiler: /usr/bin/c++ -- works
    -- Detecting CXX compiler ABI info
    -- Detecting CXX compiler ABI info - done
    -- Detecting CXX compile features
    -- Detecting CXX compile features - done
    -- Check for working C compiler: /usr/bin/cc
    -- Check for working C compiler: /usr/bin/cc -- works
    -- Detecting C compiler ABI info
    -- Detecting C compiler ABI info - done
    -- Detecting C compile features
    -- Detecting C compile features - done
    -- Build type not specified: defaulting to release.
    -- Boost version: 1.65.1
    -- Found the following Boost libraries:
    --   filesystem
    --   system
    -- Found Armadillo: /usr/lib/x86_64-linux-gnu/libarmadillo.so (found suitable version "12.0.1", minimum required is "7.300") 
    -- Armadillo found
    -- Found PkgConfig: /usr/bin/pkg-config (found version "0.29.1") 
    -- Checking for module 'cppunit'
    --   Found cppunit, version 1.14.0
    -- Found CPPUNIT: /usr/lib/x86_64-linux-gnu/libcppunit.so;dl  
    -- Found Doxygen: /usr/bin/doxygen (found version "1.8.13") found components:  doxygen missing components:  dot
    Checking for GNU Radio Module: RUNTIME
    -- Checking for module 'gnuradio-runtime'
    --   Found gnuradio-runtime, version 3.7.14.0
     * INCLUDES=/usr/local/include
     * LIBS=/usr/local/lib/libgnuradio-runtime.so;/usr/local/lib/libgnuradio-pmt.so
    -- Found GNURADIO_RUNTIME: /usr/local/lib/libgnuradio-runtime.so;/usr/local/lib/libgnuradio-pmt.so  
    GNURADIO_RUNTIME_FOUND = TRUE
    -- 
    -- Checking for module SWIG
    -- Found SWIG version 3.0.12.
    -- Found SWIG: /usr/bin/swig3.0  
    -- Found PythonLibs: /usr/lib/x86_64-linux-gnu/libpython2.7.so (found suitable version "2.7.17", minimum required is "2") 
    -- Looking for sys/types.h
    -- Looking for sys/types.h - found
    -- Looking for stdint.h
    -- Looking for stdint.h - found
    -- Looking for stddef.h
    -- Looking for stddef.h - found
    -- Check size of size_t
    -- Check size of size_t - done
    -- Check size of unsigned int
    -- Check size of unsigned int - done
    -- Performing Test HAVE_WNO_UNUSED_BUT_SET_VARIABLE
    -- Performing Test HAVE_WNO_UNUSED_BUT_SET_VARIABLE - Success
    -- Configuring done
    -- Generating done
    -- Build files have been written to: /home/ennio/github/gr-doa/build

    Then make:

    Scanning dependencies of target gnuradio-doa
    Scanning dependencies of target _doa_swig_doc_tag
    Scanning dependencies of target pygen_python_a88e3
    [  4%] Building CXX object swig/CMakeFiles/_doa_swig_doc_tag.dir/_doa_swig_doc_tag.cpp.o
    [  8%] Generating __init__.pyc, phase_correct_hier.pyc, average_and_save.pyc, compass.pyc, save_antenna_calib.pyc, twinrx_phase_offset_est.pyc, findmax_and_save.pyc
    [ 13%] Linking CXX executable _doa_swig_doc_tag
    [ 17%] Generating __init__.pyo, phase_correct_hier.pyo, average_and_save.pyo, compass.pyo, save_antenna_calib.pyo, twinrx_phase_offset_est.pyo, findmax_and_save.pyo
    [ 21%] Building CXX object lib/CMakeFiles/gnuradio-doa.dir/autocorrelate_impl.cc.o
    [ 21%] Built target _doa_swig_doc_tag
    Scanning dependencies of target pygen_apps_9a6dd
    [ 21%] Built target pygen_apps_9a6dd
    Scanning dependencies of target doxygen_target
    [ 26%] Generating documentation with doxygen
    warning: Tag `XML_SCHEMA' at line 1511 of file `/home/ennio/github/gr-doa/build/docs/doxygen/Doxyfile' has become obsolete.
             To avoid this warning please remove this line from your configuration file or upgrade it using "doxygen -u"
    warning: Tag `XML_DTD' at line 1517 of file `/home/ennio/github/gr-doa/build/docs/doxygen/Doxyfile' has become obsolete.
             To avoid this warning please remove this line from your configuration file or upgrade it using "doxygen -u"
    [ 26%] Built target pygen_python_a88e3
    Scanning dependencies of target doa_swig_swig_doc
    [ 30%] Generating doxygen xml for doa_swig_doc docs
    This is pdfTeX, Version 3.14159265-2.6-1.40.18 (TeX Live 2017/Debian) (preloaded format=latex)
     restricted \write18 enabled.
    entering extended mode
    (./_formulas.tex
    LaTeX2e <2017-04-15>
    Babel <3.18> and hyphenation patterns for 3 language(s) loaded.
    warning: Tag `XML_SCHEMA' at line 1478 of file `/home/ennio/github/gr-doa/build/swig/doa_swig_doc_swig_docs/Doxyfile' has become obsolete.
             To avoid this warning please remove this line from your configuration file or upgrade it using "doxygen -u"
    warning: Tag `XML_DTD' at line 1484 of file `/home/ennio/github/gr-doa/build/swig/doa_swig_doc_swig_docs/Doxyfile' has become obsolete.
             To avoid this warning please remove this line from your configuration file or upgrade it using "doxygen -u"
    (/usr/share/texlive/texmf-dist/tex/latex/base/article.cls
    Document Class: article 2014/09/29 v1.4h Standard LaTeX document class
    (/usr/share/texlive/texmf-dist/tex/latex/base/size10.clo))
    (/usr/share/texlive/texmf-dist/tex/latex/graphics/epsfig.sty
    (/usr/share/texlive/texmf-dist/tex/latex/graphics/graphicx.sty
    (/usr/share/texlive/texmf-dist/tex/latex/graphics/keyval.sty)
    (/usr/share/texlive/texmf-dist/tex/latex/graphics/graphics.sty
    (/usr/share/texlive/texmf-dist/tex/latex/graphics/trig.sty)
    (/usr/share/texlive/texmf-dist/tex/latex/graphics-cfg/graphics.cfg)
    (/usr/share/texlive/texmf-dist/tex/latex/graphics-def/dvips.def))))
    No file _formulas.aux.
    [1] [2] [3] [4] [5] [6] [7] [8] [9] [10] [11] [12] [13] [14] [15] [16] [17]
    [18] [19] [20] [21] [22] [23] [24] [25] [26] [27] [28] [29] [30] [31] [32]
    [33] [34] [35] [36] [37] [38] [39] [40] [41] [42] [43] [44] [45] [46] [47]
    [48] [49] [50] [51] (./_formulas.aux) )
    Output written on _formulas.dvi (51 pages, 7460 bytes).
    Transcript written on _formulas.log.
    [ 34%] Generating python docstrings for doa_swig_doc
    [ 34%] Built target doa_swig_swig_doc
    Scanning dependencies of target _doa_swig_swig_tag
    [ 39%] Building CXX object swig/CMakeFiles/_doa_swig_swig_tag.dir/_doa_swig_swig_tag.cpp.o
    [ 43%] Linking CXX executable _doa_swig_swig_tag
    [ 43%] Built target _doa_swig_swig_tag
    [ 47%] Generating doa_swig.tag
    Scanning dependencies of target doa_swig_swig_2d0df
    [ 52%] Building CXX object swig/CMakeFiles/doa_swig_swig_2d0df.dir/doa_swig_swig_2d0df.cpp.o
    [ 56%] Linking CXX executable doa_swig_swig_2d0df
    Swig source
    [ 56%] Built target doa_swig_swig_2d0df
    Scanning dependencies of target pygen_swig_13be6
    [ 60%] Generating doa_swig.pyc
    [ 65%] Generating doa_swig.pyo
    [ 65%] Built target pygen_swig_13be6
    [ 69%] Building CXX object lib/CMakeFiles/gnuradio-doa.dir/MUSIC_lin_array_impl.cc.o
    [ 69%] Built target doxygen_target
    [ 73%] Building CXX object lib/CMakeFiles/gnuradio-doa.dir/rootMUSIC_linear_array_impl.cc.o
    [ 78%] Building CXX object lib/CMakeFiles/gnuradio-doa.dir/antenna_correction_impl.cc.o
    [ 82%] Building CXX object lib/CMakeFiles/gnuradio-doa.dir/find_local_max_impl.cc.o
    [ 86%] Building CXX object lib/CMakeFiles/gnuradio-doa.dir/calibrate_lin_array_impl.cc.o
    [ 91%] Linking CXX shared library libgnuradio-doa.so
    [ 91%] Built target gnuradio-doa
    Scanning dependencies of target _doa_swig
    [ 95%] Building CXX object swig/CMakeFiles/_doa_swig.dir/doa_swigPYTHON_wrap.cxx.o
    [100%] Linking CXX shared module _doa_swig.so
    [100%] Built target _doa_swig
    

    Finally, make test

    Running tests...
    Test project /home/ennio/github/gr-doa/build
        Start 1: qa_autocorrelate
    1/5 Test #1: qa_autocorrelate .................***Failed    5.90 sec
        Start 2: qa_MUSIC_lin_array
    2/5 Test #2: qa_MUSIC_lin_array ...............   Passed   11.93 sec
        Start 3: qa_rootMUSIC_linear_array
    3/5 Test #3: qa_rootMUSIC_linear_array ........   Passed    6.66 sec
        Start 4: qa_find_local_max
    4/5 Test #4: qa_find_local_max ................***Failed    2.36 sec
        Start 5: qa_calibrate_lin_array
    5/5 Test #5: qa_calibrate_lin_array ...........***Failed   22.09 sec
    
    40% tests passed, 3 tests failed out of 5
    
    Total Test time (real) =  48.95 sec
    
    The following tests FAILED:
    	  1 - qa_autocorrelate (Failed)
    	  4 - qa_find_local_max (Failed)
    	  5 - qa_calibrate_lin_array (Failed)
    Errors while running CTest
    Makefile:85: recipe for target 'test' failed
    make: *** [test] Error 8

    Is this something I have to worry about?

    Thanks

    Ennio

  • The tests were simply forked from the upstream repo and never touched. From what I remember you need very specific versions of octave and its toolboxes for that tests to function. Those versions are in the readme.

    -Travis

  • Ok, the tool seems to be installed correctly.

    Now I want to check the RX stream from channels 1 and 2 but when running this simple flowgraph

    GR returns the following errors:

    Unable to write attribute in_voltage0_hardwaregain: -95
    Unable to write attribute in_voltage1_hardwaregain: -95
    Unable to write attribute in_voltage0_hardwaregain: -95
    Unable to write attribute in_voltage1_hardwaregain: -95
    ERROR: WRITE ALL: -9

    I have libiio v0.24-20-gfdecc362 and libad9361 checked out on 2018_R2.

  • That error would only happen if you set the Gain Mode to 'manual' and the gains to 95, which is out of range. Is that screenshot the configuration you ran? If you can to provide the flowgraph that would be helpful.

    -Travis

Reply Children
  • Is that screenshot the configuration you ran?

    Yes. Anyway, now the error isn't returned anymore and I can see the waveforms correctly.

    Another error arises when running this

    to measure the phase shift between two channels. GR returns "ERROR: WRITE ALL: -9" and even though the execution isn't stopped, the results are unreliable (i.e. the phase shift between two channels of the same chip is bigger than that of two channels of different uncalibrated chips).