All -
With help on the Linux driver forum, I was able to get a device tree configuration working that helps get data from my ADIS16485 mounted on the EVAL-RPIZ board, on the Raspberry Pi 4B. Good so far.
Was able to use the pyadi-iio module to actually get the six channels of IMU data from the subject IMU. Was using the adis16495 support from the module, and data comes through. Good.
Wanted to get the temp0 and timestamp channels, but the '495 module didn't have those, explicitly rejecting the requests for more channels beyond the IIO channel indices 0-5 and/or the named channels 'temp0' and 'timestamp'. Running the 'iio_info' command shows the two extra channels to be available from the Linux IIO subsystem. So, copied module adis16495.py -> adis16485.py and added the channels (simple change from the '495 file), placing it in the support folder. Good, now the channels are allowed. However, the data coming from those two channels doesn't match the data that the IIO Scope shows (well, at least the temperature channel), not looking anything as expected for those channels.
I note that the indices provided by iio_info are 0-5 (imu), 7 (timestamp), and 10 (temp0). Do I need to be feeding more to the adis Python module so that it knows which indices it should be seeking? Seems like it should be able to (or does) get all it needs from the Linux IIO layer to figure this out already.
Other thoughts or recommendations?
For ref, here's the output from 'iio_info':
analog@analog:~/Logger $ iio_info
Library version: 0.24 (git tag: accb7b5)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.24 (git tag: accb7b5)
Backend description string: Linux analog 5.10.63-v7l+ #1 SMP Wed Dec 21 12:09:15 UTC 2022 armv7l
IIO context has 4 attributes:
hw_carrier: Raspberry Pi 4 Model B Rev 1.2
dtoverlay: vc4-kms-v3d,adis16485
local,kernel: 5.10.63-v7l+
uri: local:
IIO context has 6 devices:
hwmon0: cpu_thermal
1 channels found:
temp1: (input)
1 channel-specific attributes found:
attr 0: input value: 56965
No trigger on this device
hwmon1: rpi_volt
1 channels found:
in0: (input)
1 channel-specific attributes found:
attr 0: lcrit_alarm value: 0
No trigger on this device
hwmon2: hidpp_battery_0
0 channels found:
No trigger on this device
iio:device0: adis16485 (buffer capable)
8 channels found:
anglvel_x: (input, index: 0, format: be:S32/32>>0)
5 channel-specific attributes found:
attr 0: calibbias value: 0
attr 1: calibscale value: 0
attr 2: filter_low_pass_3db_frequency value: 0
attr 3: raw value: -1111592
attr 4: scale value: 0.000000005
anglvel_y: (input, index: 1, format: be:S32/32>>0)
5 channel-specific attributes found:
attr 0: calibbias value: 0
attr 1: calibscale value: 0
attr 2: filter_low_pass_3db_frequency value: 0
attr 3: raw value: -345410
attr 4: scale value: 0.000000005
anglvel_z: (input, index: 2, format: be:S32/32>>0)
5 channel-specific attributes found:
attr 0: calibbias value: 0
attr 1: calibscale value: 0
attr 2: filter_low_pass_3db_frequency value: 0
attr 3: raw value: 1367883
attr 4: scale value: 0.000000005
accel_x: (input, index: 3, format: be:S32/32>>0)
5 channel-specific attributes found:
attr 0: calibbias value: 0
attr 1: calibscale value: 0
attr 2: filter_low_pass_3db_frequency value: 0
attr 3: raw value: -18474238
attr 4: scale value: 0.000000037
accel_y: (input, index: 4, format: be:S32/32>>0)
5 channel-specific attributes found:
attr 0: calibbias value: 0
attr 1: calibscale value: 0
attr 2: filter_low_pass_3db_frequency value: 0
attr 3: raw value: -13953978
attr 4: scale value: 0.000000037
accel_z: (input, index: 5, format: be:S32/32>>0)
5 channel-specific attributes found:
attr 0: calibbias value: 0
attr 1: calibscale value: 0
attr 2: filter_low_pass_3db_frequency value: 0
attr 3: raw value: 260777763
attr 4: scale value: 0.000000037
timestamp: (input, index: 7, format: le:S64/64>>0)
temp0: (input, index: 10, format: be:S16/16>>0)
3 channel-specific attributes found:
attr 0: offset value: 4425
attr 1: raw value: 4162
attr 2: scale value: 5.650000
2 device-specific attributes found:
attr 0: current_timestamp_clock value: realtime
attr 1: sampling_frequency value: 2460.000000
1 buffer-specific attributes found:
attr 0: data_available value: 26
Current trigger: trigger0(adis16485-dev0)
iio_sysfs_trigger:
0 channels found:
2 device-specific attributes found:
attr 0: add_trigger ERROR: Permission denied (13)
attr 1: remove_trigger ERROR: Permission denied (13)
No trigger on this device
trigger0: adis16485-dev0
0 channels found:
No trigger on this device
Thanks,
Andrew