The MATLAB error message I receive is:
>> rx = adi.XXXXXXX.Rx('uri','ip:169.254.17.222')
Error using adi.XXXXXXX.Rx
The specified superclass 'matlabshared.libiio.base' contains a parse error, cannot be found on MATLAB's search path, or is shadowed by another file with the same name.
The ‘Data Streaming with Hardware’ dependencies have been installed successfully:
- AnalogDevicesHighSpeedConverterToolbox_v21.2.1.mltbx
- libiio MATLAB Binding Standalone Installer (R2021b+): Libiio.mlpkginstall is required but not available to install offline.
- Installed libiio-v2.4-setup.exe but does not have the right files for MATLAB
I cannot find an MATLAB offline installer for Libiio.mlpkginstall, even though it states "standalone" on website.
It has references to 'Signal Processing Toolbox Support Package for Linux IIO Devices' in the MathWorks repository, but no way to download this without the computer connected to the internet.
Please can the 'Signal Processing Toolbox Support Package for Linux IIO Devices'' hardware support package for MATLAB be supplied as an offline installer?
Thanks in advance.
Sunny