Post Go back to editing

pyadi-jif usage: no solutions found in default example (known good config)

Category: Software
Software Version: pyadi-jif main branch, commit 631d1bc

Hi,

I am trying to use pyadi-jif to validate JESD settings for my ZCU102 <-> AD9081 FMC eval board. 

Using ad9081_rxtx_hmc7044.py, some configurations which I think should pass can't find a solution.

Notably, the code (unchanged) from github configures for JESD204C, TX Mode 0, RX Mode 1.0, as below:

sys.fpga.setup_by_dev_kit_name("zcu102")
sys.fpga.sys_clk_select = "GTH34_SYSCLK_QPLL0"  # Use faster QPLL
sys.Debug_Solver = True
sys.converter.clocking_option = "integrated_pll"
sys.fpga.out_clk_select = "XCVR_REFCLK"  # force reference to be core clock rate
sys.converter.adc.sample_clock = 2900000000 / (8 * 6)
sys.converter.dac.sample_clock = 5800000000 / (4 * 12)

sys.converter.adc.decimation = 8 * 6
sys.converter.dac.interpolation = 4 * 12

mode_tx = "0"
mode_rx = "1.0"

This matches the configuration that is set up in the latest boot configuration:
/latest_boot_partition/zynqmp-zcu102-rev10-ad9081/204c_txmode0_rxmode1

Booting with this I can see the JESD link is happy.  However, the JIF tool tells me there is no solution. 

Is there some user error here?  Any advice appreciated.

Thanks!

Matt

Parents Reply Children
No Data