I was trying to boot openwifi on my ADRV9364-Z7020 with FMC carrier board. When i try using bootfiles provided on open-wifi page. After few tries it just goes into zynq boot mode . I have attched a copy of response below. Iwant to be able to run ssh commands and use openwifi.
U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21)
Board: Xilinx Zynq
I2C: ready
DRAM: ECC disabled 512 MiB
MMC: zynq_sdhci: 0
SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB
In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 0
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5344
Name: SD64G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 59.5 GiB
Bus Width: 4-bit
Unknown command 'load' - try 'help'
Copying Linux from SD to RAM...
Unknown command 'load' - try 'help'
switch to partitions #0, OK
mmc0 is current device
Unknown command 'part' - try 'help'
env - environment handling commands
Usage:
env default [-f] -a - [forcibly] reset default environment
env default [-f] var [...] - [forcibly] reset variable(s) to their default values
env delete [-f] var [...] - [forcibly] delete variable(s)
env edit name - edit environment variable
env export [-t | -b | -c] [-s size] addr [var ...] - export environment
env import [-d] [-t | -b | -c] addr [size] - import environment
env print [-a | name ...] - print environment
env run var [...] - run commands in an environment variable
env save - save environment
env set [-f] name [arg ...]
Unknown command 'fstype' - try 'help'
(Re)start USB...
USB0: USB EHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
USB1: usb1 wrong num MIO: 0, Index 1
lowlevel init failed
scanning usb for storage devices... 0 Storage Device(s) found
USB device 0: unknown device
(Re)start USB...
USB0: USB EHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
USB1: usb1 wrong num MIO: 0, Index 1
lowlevel init failed
scanning usb for storage devices... 0 Storage Device(s) found
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Unknown command 'pxe' - try 'help'
(Re)start USB...
USB0: USB EHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
USB1: usb1 wrong num MIO: 0, Index 1
lowlevel init failed
scanning usb for storage devices... 0 Storage Device(s) found
Gem.e000b000:0 is connected to Gem.e000b000. Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
Gem.e000b000:0 is connected to Gem.e000b000. Reconnecting to Gem.e000b000
Gem.e000b000 Waiting for PHY auto negotiation to complete......... TIMEOUT !
Gem.e000b000: No link.
zynq-uboot>