Post Go back to editing

Problems using ADALM-PLUTO in python

Category: Software
Product Number: ADALM-PLUTO

Dear support team,

I want to use ADALM-PLUTO in python.

But when I use the provided pyadi-iio, I get an error.

C:\Work\python\sdr>python
Python 3.7.9 (tags/v3.7.9:13c94747c7, Aug 17 2020, 18:58:18) [MSC v.1900 64 bit (AMD64)] on win32
Type "help", "copyright", "credits" or "license" for more information.
>>> import adi
>>> sdr = adi.Pluto("ip:192.168.2.1")
Fatal: program compiled against libxml 20 using libxml 2
Fatal: program compiled against libxml 20 using libxml 2
Warning: program compiled against libxml 2090 using older 209
>>>

What's wrong?

Parents Reply
  • Michael was referring to if one existed in a local folder like C:\Work\python\sdr.

    My guess is that you just have an older version of the libxml.dll that was there before libiio was installed. The installer does not overwrite the DLL if one exists.

    I would try renaming that DLL to libxml_old.dll and reinstalling libiio through the provided exe.

    -Travis

Children
No Data