Post Go back to editing

Problem in calculating Peak Search Algorithm for RF Signal targeting ADRV9361-z7035

Category: Hardware
Product Number: ADRV9361-z7035
Software Version: HDL 2019_r2

Dear All,

I implemented a peak search algorithm in HDL reference design  targeting platform is ADI ADRV9361-z7035 . Let me first talk about my algorithm.

1-  I am calculating bin from Xilinx FFT core ( 8192 points ) inserted in ADC path

2- Then I slice 32 bit output data coming from FFT into 16 bit slice into I and Q , multiplying I*I and Q*Q and add I2+Q2 . This gave me a scalar magnitude 

3- Then I compare this scalar magnitude with a threshold ( I am giving this from VIO) . and if RF-IN is very strong ( upto -30 dBm) this algorithm give me the correct index but if signal is weaker than -30 dBm then I am getting garbage value and incorrect index

Problem 

The board is capable to detect weak signal as much as -90dBm as i confirmed by using ADI built-in IIO Oscilloscope  but here I got peak only for very strong signal and garbage and incorrect index for weaker signal .

is there any better way to calculate peak or any suggestion to improve this logic .

 

Best Regards

Parents Reply Children
  • It sounds like you are comparing input signals on logarithmic scales to a linear output of the FFT directly. So small changes in input power in reference to dBm will be large changes in your linear FFT data. Consider doing a logarithm conversion.

    I would recommend simulating these scenarios and checking the output scale has enough dynamic range to handle your desirable operational range.

    -Travis