Hi,
I have the installed pyadi-iio Python library in various Windows 10 devices to use a set of PlutoSDRs, but I always end up getting the following error:
File "C:\Users\user\anaconda3\lib\ctypes\__init__.py", line 363, in __init__
if '/' in name or '\\' in name:
TypeError: argument of type 'NoneType' is not iterable
This problem disappeared on two devices, not sure why, but it stays present on the rest of the devices and I am thus unable to use my PlutoSDRs on these devices as a result.
I was hoping somebody knows if this is a common issue or if somebody managed to fix this in the past.
Cheers!
DBK