RX LO 2000000000
Traceback (most recent call last):
File "pluto.py", line 66, in <module>
sdr.tx(iq)
File "/usr/local/lib/python3.8/dist-packages/pyadi_iio-0.0.9-py3.8.egg/adi/rx_tx.py", line 396, in tx
File "/usr/local/lib/python3.8/dist-packages/pyadi_iio-0.0.9-py3.8.egg/adi/rx_tx.py", line 331, in _tx_init_channels
File "/usr/local/lib/python3.8/dist-packages/iio.py", line 1013, in __init__
self._ctx = device.ctx()
TypeError: 'Context' object is not callable
Using Python3 on Ubuntu 20 LTS
There is a known issue with the python bindings from libiio.
Can you try downgrading pylibiio first by running:
sudo pip3 install pylibiio==0.21.0 --no-binary :all:
-Travis
There is a known issue with the python bindings from libiio.
Can you try downgrading pylibiio first by running:
sudo pip3 install pylibiio==0.21.0 --no-binary :all:
-Travis
Hi thanks for quick help and fix..
Collecting pylibiio==0.21.0
Downloading pylibiio-0.21.tar.gz (12 kB)
Skipping wheel build for pylibiio, due to binaries being disabled for it.
Installing collected packages: pylibiio
Attempting uninstall: pylibiio
Found existing installation: pylibiio 0.21.1
Uninstalling pylibiio-0.21.1:
Successfully uninstalled pylibiio-0.21.1
Running setup.py install for pylibiio ... done
Successfully installed pylibiio-0.21
Hi,
raise OSError(err, _strerror(err))
OSError: [Errno 16] Device or resource busy
coming up this error...
python 3.8.10 (default, Jun 2 2021, 10:49:15)
[GCC 9.4.0] on linux
Type "help", "copyright", "credits" or "license" for more information.
>>> import adi
>>> sdr = adi.Pluto('ip:192.168.2.1') # or whatever your Pluto's IP is
>>> sdr.sample_rate = int(2.5e6)
>>> sdr.rx()
ERROR: Open unlocked: -16
Traceback (most recent call last):
File "<stdin>", line 1, in <module>
File "/usr/local/lib/python3.8/dist-packages/pyadi_iio-0.0.9-py3.8.egg/adi/rx_tx.py", line 252, in rx
File "/usr/local/lib/python3.8/dist-packages/pyadi_iio-0.0.9-py3.8.egg/adi/rx_tx.py", line 173, in __rx_complex
File "/usr/local/lib/python3.8/dist-packages/pyadi_iio-0.0.9-py3.8.egg/adi/rx_tx.py", line 129, in _rx_init_channels
File "/usr/local/lib/python3.8/dist-packages/iio.py", line 1010, in __init__
self._buffer = _create_buffer(device._device, samples_count, cyclic)
File "/usr/local/lib/python3.8/dist-packages/iio.py", line 64, in _check_null
raise OSError(err, _strerror(err))
OSError: [Errno 16] Device or resource busy
Do you have another application like IIO-Scope running alongside pyadi?
-Travis
Hi, No i don't have any other application running if so sdr = adi.Pluto('ip:192.168.2.1') shouldn't working. i am using pluto web fw.
ps -a | grep py*
2301 pts/0 00:00:00 sudo
2305 pts/0 00:00:00 python3
3540 pts/1 00:00:00 ping
4837 pts/1 00:00:00 ps
4838 pts/1 00:00:00 grep
Can you run and return the output:
iio_readdev -u ip:192.168.2.1 cf-ad9361-lpc -s 1024 > d.dat
ls -ls d.dat
-Travis
Hi,
iio_readdev -u ip:192.168.2.1 cf-ad9361-lpc -s 1024 > d.dat
ERROR: Open unlocked: -16
Unable to allocate buffer: Device or resource busy (16)
ssh root@192.168.2.1
The authenticity of host '192.168.2.1 (192.168.2.1)' can't be established.
ECDSA key fingerprint is SHA256:OxqSaO9GsDbBiWRHlLi3/DOqpb6A8YreUViW8WnKfnk.
Are you sure you want to continue connecting (yes/no/[fingerprint])? yes
Warning: Permanently added '192.168.2.1' (ECDSA) to the list of known hosts.
root@192.168.2.1's password:
Welcome to:
______ _ _ _________________
| ___ \ | | | / ___| _ \ ___ \
| |_/ / |_ _| |_ ___ \ `--.| | | | |_/ /
| __/| | | | | __/ _ \ `--. \ | | | /
| | | | |_| | || (_) /\__/ / |/ /| |\ \
\_| |_|\__,_|\__\___/\____/|___/ \_| \_|
v0.30-27-gd5bb-dirty
wiki.analog.com/.../pluto
PlutoWeb v3.0
http://pluto.local/
Run settings.sh to see available options.
Dual-core enabled
70-6000Mhz range enabled
Auto-reboot disabled
Auto-updates disabled
This is not related to pyadi. Can you re-plugin Pluto and/or reboot your machine?
-Travis