Stream data into/out of MATLAB

Hi ,

 

I want to Stream data into/out of MATLAB

With your tools so I started with the following link:

https://wiki.analog.com/resources/tools-software/transceiver-toolbox

 

I then performed the following steps:

I use windows.

And I installed the

MATLAB R2020a

Xilinx Vivado 2018.2

AnalogDevicesTransceiverToolbox_v20.1.1.mltbx

 

I installed Libiio Installers

 

Now I'm trying to figure out what I should have in SD CARD if at all?

 

 

I am using ZC706 + AD9361

 

Thanks for your help

  • Hi Travis 

    thanks for the response 

    yes, it boot correctly

    thanks

    Ron

  • Hi Travis ,

    Do you have any suggestions for a solution?

    Maybe something to do with incompatible versions?
    Maybe you want me to try another example?

  • 0
    •  Analog Employees 
    on Apr 9, 2021 4:51 PM in reply to ron1

    Can you export the HDL Workflow Advisor configuration as a script and post it here?

    -Travis

  • yes

    %--------------------------------------------------------------------------
    % HDL Workflow Script
    % Generated with MATLAB 9.8 (R2020a) at 13:16:17 on 10/04/2021
    % This script was generated using the following parameter values:
    % Filename : 'C:\tr_toolbox\hdlworkflow.m'
    % Overwrite : true
    % Comments : true
    % Headers : true
    % DUT : 'ModeS_ADI_Codegen/Detector'
    % To view changes after modifying the workflow, run the following command:
    % >> hWC.export('DUT','ModeS_ADI_Codegen/Detector');
    %--------------------------------------------------------------------------

    %% Load the Model
    load_system('ModeS_ADI_Codegen');

    %% Restore the Model to default HDL parameters
    %hdlrestoreparams('ModeS_ADI_Codegen/Detector');

    %% Model HDL Parameters
    %% Set Model 'ModeS_ADI_Codegen' HDL parameters
    hdlset_param('ModeS_ADI_Codegen', 'Backannotation', 'on');
    hdlset_param('ModeS_ADI_Codegen', 'CodeGenerationOutput', 'GenerateHDLCodeAndDisplayGeneratedModel');
    hdlset_param('ModeS_ADI_Codegen', 'HDLSubsystem', 'ModeS_ADI_Codegen/Detector');
    hdlset_param('ModeS_ADI_Codegen', 'OptimizationReport', 'on');
    hdlset_param('ModeS_ADI_Codegen', 'ReferenceDesign', 'FMCOMMS2/3 ZC706 (RX)');
    hdlset_param('ModeS_ADI_Codegen', 'ResourceReport', 'on');
    hdlset_param('ModeS_ADI_Codegen', 'SynthesisTool', 'Xilinx Vivado');
    hdlset_param('ModeS_ADI_Codegen', 'SynthesisToolChipFamily', 'Zynq');
    hdlset_param('ModeS_ADI_Codegen', 'SynthesisToolDeviceName', 'xc7z045');
    hdlset_param('ModeS_ADI_Codegen', 'SynthesisToolPackageName', 'ffg900');
    hdlset_param('ModeS_ADI_Codegen', 'SynthesisToolSpeedValue', '-2');
    hdlset_param('ModeS_ADI_Codegen', 'TargetDirectory', 'C:\tr_toolbox\hdl_prj\hdlsrc');
    hdlset_param('ModeS_ADI_Codegen', 'TargetLanguage', 'Verilog');
    hdlset_param('ModeS_ADI_Codegen', 'TargetPlatform', 'AnalogDevices FMCOMMS2/3 ZC706');
    hdlset_param('ModeS_ADI_Codegen', 'Traceability', 'on');
    hdlset_param('ModeS_ADI_Codegen', 'Workflow', 'IP Core Generation');

    % Set SubSystem HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector', 'AXI4SlaveIDWidth', '12');
    hdlset_param('ModeS_ADI_Codegen/Detector', 'ProcessorFPGASynchronization', 'Free running');

    % Set Inport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/I_In', 'IOInterface', 'AD9361 ADC Data I0 [0:15]');
    hdlset_param('ModeS_ADI_Codegen/Detector/I_In', 'IOInterfaceMapping', '[0:15]');

    % Set Inport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/Q_In', 'IOInterface', 'AD9361 ADC Data Q0 [0:15]');
    hdlset_param('ModeS_ADI_Codegen/Detector/Q_In', 'IOInterfaceMapping', '[0:15]');

    % Set S-Function HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/CalcNF/NoiseFloor', 'AddPipelineRegisters', 'on');
    hdlset_param('ModeS_ADI_Codegen/Detector/CalcNF/NoiseFloor', 'MultiplierOutputPipeline', 1);

    % Set S-Function HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/CalcSyncCorr/SyncCorr', 'AddPipelineRegisters', 'on');
    hdlset_param('ModeS_ADI_Codegen/Detector/CalcSyncCorr/SyncCorr', 'MultiplierOutputPipeline', 1);

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/reset', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/reset', 'IOInterfaceMapping', 'x"100"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/bit_process', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/bit_process', 'IOInterfaceMapping', 'x"104"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/empty_reg', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/empty_reg', 'IOInterfaceMapping', 'x"108"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/bit_clk', 'IOInterface', 'IP Data Valid OUT');
    hdlset_param('ModeS_ADI_Codegen/Detector/bit_clk', 'IOInterfaceMapping', '[0]');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/bits', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/bits', 'IOInterfaceMapping', 'x"10C"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/crc', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/crc', 'IOInterfaceMapping', 'x"110"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/noise_floor', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/noise_floor', 'IOInterfaceMapping', 'x"114"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/sync_corr', 'IOInterface', 'AXI4');
    hdlset_param('ModeS_ADI_Codegen/Detector/sync_corr', 'IOInterfaceMapping', 'x"118"');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/data', 'IOInterface', 'IP Data 0 OUT [0:15]');
    hdlset_param('ModeS_ADI_Codegen/Detector/data', 'IOInterfaceMapping', '[0:15]');

    % Set Outport HDL parameters
    hdlset_param('ModeS_ADI_Codegen/Detector/frame_valid', 'IOInterface', 'IP Data 1 OUT [0:15]');
    hdlset_param('ModeS_ADI_Codegen/Detector/frame_valid', 'IOInterfaceMapping', '[0:15]');


    %% Workflow Configuration Settings
    % Construct the Workflow Configuration Object with default settings
    hWC = hdlcoder.WorkflowConfig('SynthesisTool','Xilinx Vivado','TargetWorkflow','IP Core Generation');

    % Specify the top level project directory
    hWC.ProjectFolder = 'C:\tr_toolbox\hdl_prj';
    hWC.ReferenceDesignToolVersion = '2018.2';
    hWC.IgnoreToolVersionMismatch = false;

    % Set Workflow tasks to run
    hWC.RunTaskGenerateRTLCodeAndIPCore = true;
    hWC.RunTaskCreateProject = true;
    hWC.RunTaskGenerateSoftwareInterfaceModel = true;
    hWC.RunTaskBuildFPGABitstream = true;
    hWC.RunTaskProgramTargetDevice = false;

    % Set properties related to 'RunTaskGenerateRTLCodeAndIPCore' Task
    hWC.IPCoreRepository = '';
    hWC.GenerateIPCoreReport = true;

    % Set properties related to 'RunTaskCreateProject' Task
    hWC.Objective = hdlcoder.Objective.None;
    hWC.AdditionalProjectCreationTclFiles = '';
    hWC.EnableIPCaching = false;

    % Set properties related to 'RunTaskGenerateSoftwareInterfaceModel' Task
    hWC.OperatingSystem = 'Linux';

    % Set properties related to 'RunTaskBuildFPGABitstream' Task
    hWC.RunExternalBuild = true;
    hWC.TclFileForSynthesisBuild = hdlcoder.BuildOption.Custom;
    hWC.CustomBuildTclFile = 'C:\tr_toolbox\hdl_prj\vivado_ip_prj\projects\scripts\adi_build.tcl';

    % Set properties related to 'RunTaskProgramTargetDevice' Task
    hWC.ProgrammingMethod = hdlcoder.ProgrammingMethod.Download;

    % Validate the Workflow Configuration Object
    hWC.validate;

    %% Run the workflow
    hdlcoder.runWorkflow('ModeS_ADI_Codegen/Detector', hWC);

  • Hi Travis,


    Can I perhaps pass on more information that can help solve my problem?

    Maybe try running on a different example or version?

    thanks

    Ron