Hello,
I am trying to download the new pre_release files for ADRV9002/ZCU102 as I currently have an older revision.
I downloaded the files from http://swdownloads.analog.com/cse/tmp/B0_2019_r2_pre_release_zcu102.zip and put them on my SD card.
In the base directory of my SD card I have only the following files that were downloaded from the above zip.
BOOT.BIN
Image
uEnv.txt
system_split.dtb
When I boot the ZCU102 with the new SD card, I get all green lights on the ZCU102 but over the COM port via the UART I get the following messages from the ZYNC:
ZynqMP> Xilinx Zynq MP First Stage Boot Loader
Release 2019.1 Feb 19 2021 - 17:54:45
NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE: BL31: Secure code at 0x0
NOTICE: BL31: Non secure code at 0x8000000
NOTICE: BL31: v2.0(release):xilinx-v2019.2
NOTICE: BL31: Built : 10:19:24, Jan 13 2020
PMUFW: v1.1
U-Boot 2018.01-21436-gbba91bc203 (Jan 13 2020 - 10:50:58 +0200) Xilinx ZynqMP ZCU102 rev1.0, Build: jenkins-development-build_uboot-1
I2C: ready
DRAM: 4 GiB
EL Level: EL2
Chip ID: zu9eg
MMC: sdhci@ff170000: 0 (SD)
*** Warning - bad CRC, using default environment
In: serial@ff000000
Out: serial@ff000000
Err: serial@ff000000
Bootmode: LVL_SHFT_SD_MODE1
Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id
Warning: ethernet@ff0e0000 using MAC address from ROM
eth0: ethernet@ff0e0000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 41
OEM: 3432
Name: SD16G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.4 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uEnv.txt
394 bytes read in 15 ms (25.4 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
** No boot file defined **
** Unable to read file system.dtb **
## Error: "distro_bootcmd" not defined
Is there a step I may be missing.
Thanks!