Post Go back to editing

Arduino uno not connect with quickeval software

Thread Summary

The user was unable to connect their Arduino Uno with an FT232RL to the QuickEval software for the LTC6804-1 battery management system. The solution involved changing the FT232RL description to 'USB SERIAL CONTROLLER' using FTprog, and modifying the 'enhanced' DC590B sketch to spoof the EEPROM ID string for the LTC6804-1. This allowed the QuickEval software to recognize and connect to the Arduino Uno, enabling the user to evaluate their custom board setup.
AI Generated Content

Hi i use a arduino uno with FT232RL from ftdi chip for convert UART to USB as Linduino use, i upload to my arduino the sketchbook DC590B and i can take the message "hello" from my serial port wich that mean sketchbook have  successfully upoload and work , but the problem is that can not connect with QuickEval software, where is the problem?

thanks

Parents
  • Hi Yiannis,

    So QuikEval and the individual, part-specific example sketches are mutually exclusive. QuikEval requires that the "DC590 emulator" sketch be loaded:

    https://github.com/analogdevicesinc/Linduino/blob/master/LTSketchbook/Utilities/DC590B/DC590B.ino

    This sketch is a command interpreter and not really useful aside from using with QuikEval.

    The idea is, get the hardware up and running with QuikEval GUI, then move on to the part-specific sketch for further application development.

    What eval board are you connecting the Linduino to? Note that QuikEval will not do anything without an additional eval board connected, as it queries an identification EEPROM. But you do say that you see the "hello" message in the terminal, which is to be expected from the DC590 emulator, so perhaps this is the problem?

    Another possibility - are you trying to run QuikEval with the Arduino terminal open? If so, the terminal will claim the USB serial port, and QuikEval won't be able to access it. Try closing the terminal, and the Arduino IDE, too, just to be extra sure.

    A screenshot, and even a photo of your setup may also help.

    -Mark

  • Realizing I overlooked the consequences of your Arduino setup. QuikEval also requires that the FTDI chip have the following string for a description:

    USB SERIAL CONTROLLER

    You would need to download the FTprog utility from FTDI to program this in. But if this does not work right away, there might be some other subtlety that I haven't thought of.

    Even after getting that sorted out, you'd need to either wire your ARduino's I2C bus to the eval board's EEPROM, or implement a hack in the DC590 emulator that's not terribly difficult, but might not be worth the effort.

    Again, depending on which part you're using, the QuikEval GUI may just be intended to show signs of life and basic functionality. (Not always true though.) The part-specific drivers and code examples tend to be much more useful. And once we know which part you're using, we can move the discussion to the appropriate product forum.

    -Mark

  • HI Mark and thanks for your help! i make the change you ask me to FT232RL and i change it from "FT232 USB UART" as was to "USB SERIAL CONTROLLER" and yes i see a difference action:
    1) first its take about 15 sec to take from QuickEval the message " The Usb to Serial controller not connected" and only RX pin of arduino led blink, before the change i take the above message in zero time like not connect nothinc on USB port.
    2) two times was connect after ten times tray and i take the message " Usb Controller connected but not board find" and disconnect after from maybe 2 or 3 seconds.

  • Hi Yiannis,

    So QuikEval is attempting to connect to a demo board, but you still have not told us what demo board you are connecting to. QuikEval will only work with certain product demo boards, and they all have an identification EEPROM that is pre-programmed when the board is tested.

    We need to know which demo board you are using, or at least which product you are attempting to communicate with.

    -Mark

  • HI MARK

    The prodcut wich tray to communicate is the ltc6804-1wich i have communicate with arduino when upload the sketchbook dc1894 and via usb i can reed the cell voltage and etc, i will send the screen shot.

    So always i have connection when upload the DC590b and take the message "HELLO"  and when upload DC1894 to my arduino i can connect with LTC6804.

    To mension when i change the description to FT232 the rx led of arduino was first time blink every time to tray to connect with QuickEval wich not happen before.

    so the problem now is that not always have connection with QuickEval wich must be and if not have any product connect to arduino to take the message " usb to serial controller has been found but the evaluthion board is not connected"

     

  • Here its some screenshot:

    arduino with DC590B

    Arduino with DC590B

    Arduino with DC1894

    Arduino with DC1894 :reed cells from LTC6804-1"

    FIRST TIME CONNECT

    First time connection with QuickEval

    USB SERIAL CONTROLLER

    FT232 change to USB SERIAL CONTROLLER

  • Here is some screenshot how EEPROM of my ft232 is:

    Thanks Mark

  • Okay now we are getting somewhere. To clarify - QuikEval requires that the DC590B emulator sketch be loaded:

    https://github.com/analogdevicesinc/Linduino/blob/master/LTSketchbook/Utilities/DC590B/DC590B.ino

    But I think you've got that right.

    Do the following - after the "hello" message, type in a lower-case "i", which should return an ID string for the DC590B sketch. NEXT - type in an UPPER-case "I", which SHOULD return an ID string from the board. But this will ONLY happen if your Arduino Uno's I2C bus is connected to the dc1894's EEPROM, and the EEPROM is powered properly. 

    So could you double-check that you've made these connections? Refer to pins 9, 10, 11, 12 on J2.

    If this does not work right away, send a photograph of your Arduino - dc1894 connections. You should use short wires, and make sure Arduino ground is well-connected to DC1894 ground.

    -Mark

  • Hi Mark and sorry for late replay!

    T

    This is a screenshot  by type "i" when DC590B scketchbook upload to arduino  without  board LTC6804 connected.

    Now i want to understant , must be type "l" when DC590B is loaded to arduino and LTC6804 board is connected ? or when DC1894 is loaded  and LTC6804 board is connected? ( i do that tomorrow because i have LTC6804 board to my job)

    Thanks a lot Mark

     
  • Hi Yiannis,

    You have the right idea - when you connect your Uno's SDA/SCL to the EEPROM on the DC1894, you should be able to execute the "I" command, and QuikEval should bring up the correct GUI.

    But I'll give you another option - occasionally we've gotten requests for a workaround so that the EEPROM is not required, as sometimes the GUI can be a useful debugging aid during development. There is an alternative "enhanced" DC590 sketch that should be backwards compatible with the standard one, which supports "spoofing" the EEPROM. See:

    https://github.com/analogdevicesinc/Linduino/blob/master/LTSketchbook/Utilities/DC590B_enhanced/DC590B_enhanced.ino#L63

    I tracked down the ID for your board, try adding this:

    //#define spoof_board_id "LTC6804-1,Cls,D6804-1,01,01,DC,DC1894A,---------"

    at line 71, then upload to your Arduino.

    If neither of these work, we'll have to move this over to the support forum for the LTC6804. And if it ends up taking too much time and effort, the best thing might be to just get an actual Linduino board.

    Mark

  • Hi Mark!

    Great success! its work!

    the first time i type with "//" and not work, after i relase my mystake and type without and work.

    I post some screenshot so another people here can help from this

    I would like to ask you aslo wich is ID for LTC6811-1 , LTC6812-1, LTC6813-1 BOARDS because i want to work with this new chips.

    Thanks a lot Mark great job! keep doing this!

Reply
  • Hi Mark!

    Great success! its work!

    the first time i type with "//" and not work, after i relase my mystake and type without and work.

    I post some screenshot so another people here can help from this

    I would like to ask you aslo wich is ID for LTC6811-1 , LTC6812-1, LTC6813-1 BOARDS because i want to work with this new chips.

    Thanks a lot Mark great job! keep doing this!

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.