ADRV9002 + zcu102 linux and GNU Radio support

Hi,

I'm using a zcu102 board with adrv9002 EVB.

I've created a SD card for this setup using the guide:

https://wiki.analog.com/resources/tools-software/linux-software/zynq_images#preparing_the_image

and set up the boot files for the appropriate configuration.

When I boot, i get a console to the linux but unable to get linux GUI. The screen is jut black and displays a single underscore character.

When I try to run "startx" from the console it freezes on "Loading Extension GLX" and nothing happens.

How can I get the GUI to run?

Also, wanted to ask is there a GNU Radio support for ADRV9002? Are there appropriate Sink/Source blocks like for fmcomms?

Thanks and BR,

Alex

Parents Reply Children
  • I've created a new SD card using

    http://swdownloads.analog.com/cse/kuiper/2021-01-21-ADI-Kuiper.img.xz

    that was in the link you provided.

    Now when i'm trying to load the profile i get the folowing message:

    root@analog:/sys/bus/iio/devices/iio:device1# cat /boot/kozlov/profile1.json > profile_config
    cat: write error: Bad address

    What am I doing wrong?

    I'm attaching the profile.

    -Alex


    profile1.zip

  • 0
    •  Analog Employees 
    on Mar 2, 2021 6:12 PM in reply to kozlova

    Can you provide the output of dmesg after writing the profile?

    -Travis

  • root@analog:/sys/bus/iio/devices/iio:device1# cat /boot/kozlov/profile1.json > profile_config
    cat: write error: Bad address
    root@analog:/sys/bus/iio/devices/iio:device1# demsg
    bash: demsg: command not found
    root@analog:/sys/bus/iio/devices/iio:device1# dmesg
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 4.19.0-g11b5080 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #960 SMP Mon Jan 25 15:45:00 GMT 2021
    [    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
    [    0.000000] bootconsole [cdns0] enabled
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
    [    0.000000] On node 0 totalpages: 1048576
    [    0.000000]   DMA32 zone: 7168 pages used for memmap
    [    0.000000]   DMA32 zone: 0 pages reserved
    [    0.000000]   DMA32 zone: 524288 pages, LIFO batch:63
    [    0.000000]   Normal zone: 7168 pages used for memmap
    [    0.000000]   Normal zone: 524288 pages, LIFO batch:63
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.
    [    0.000000] psci: SMC Calling Convention v1.1
    [    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with crng_init=0
    [    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112
    [    0.000000] pcpu-alloc: s52504 r8192 d29416 u90112 alloc=22*4096
    [    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: enabling workaround for ARM erratum 845719
    [    0.000000] Speculative Store Bypass Disable mitigation not required
    [    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
    [    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
    [    0.000000] Memory: 3772756K/4194304K available (12796K kernel code, 1538K rwdata, 13452K rodata, 832K init, 324K bss, 159404K reserved, 262144K cma-reserved)
    [    0.000000] rcu: Hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns
    [    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
    [    0.008257] Console: colour dummy device 80x25
    [    0.012390] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
    [    0.022756] pid_max: default: 32768 minimum: 301
    [    0.027448] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.034012] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.041766] ASID allocator initialised with 32768 entries
    [    0.046508] rcu: Hierarchical SRCU implementation.
    [    0.051548] EFI services will not be available.
    [    0.055826] smp: Bringing up secondary CPUs ...
    [    0.060480] Detected VIPT I-cache on CPU1
    [    0.060508] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.060807] Detected VIPT I-cache on CPU2
    [    0.060827] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.061107] Detected VIPT I-cache on CPU3
    [    0.061127] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.061170] smp: Brought up 1 node, 4 CPUs
    [    0.095681] SMP: Total of 4 processors activated.
    [    0.100354] CPU features: detected: 32-bit EL0 Support
    [    0.106757] CPU: All CPU(s) started at EL2
    [    0.109534] alternatives: patching kernel code
    [    0.114811] devtmpfs: initialized
    [    0.122372] Registered cp15_barrier emulation handler
    [    0.122419] Registered setend emulation handler
    [    0.126841] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.136436] futex hash table entries: 1024 (order: 4, 65536 bytes)
    [    0.148045] xor: measuring software checksum speed
    [    0.186638]    8regs     :  2375.000 MB/sec
    [    0.226668]    8regs_prefetch:  2052.000 MB/sec
    [    0.266697]    32regs    :  2724.000 MB/sec
    [    0.306727]    32regs_prefetch:  2308.000 MB/sec
    [    0.306767] xor: using function: 32regs (2724.000 MB/sec)
    [    0.311069] pinctrl core: initialized pinctrl subsystem
    [    0.316820] NET: Registered protocol family 16
    [    0.321042] audit: initializing netlink subsys (disabled)
    [    0.326088] audit: type=2000 audit(0.272:1): state=initialized audit_enabled=0 res=1
    [    0.333728] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
    [    0.333732] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.348488] DMA: preallocated 256 KiB pool for atomic allocations
    [    0.367176] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.436471] raid6: int64x1  gen()   444 MB/s
    [    0.504451] raid6: int64x1  xor()   451 MB/s
    [    0.572496] raid6: int64x2  gen()   679 MB/s
    [    0.640550] raid6: int64x2  xor()   600 MB/s
    [    0.708608] raid6: int64x4  gen()   981 MB/s
    [    0.776608] raid6: int64x4  xor()   737 MB/s
    [    0.844668] raid6: int64x8  gen()  1162 MB/s
    [    0.912707] raid6: int64x8  xor()   759 MB/s
    [    0.980789] raid6: neonx1   gen()   736 MB/s
    [    1.048779] raid6: neonx1   xor()   880 MB/s
    [    1.116874] raid6: neonx2   gen()  1130 MB/s
    [    1.184889] raid6: neonx2   xor()  1174 MB/s
    [    1.252950] raid6: neonx4   gen()  1479 MB/s
    [    1.320959] raid6: neonx4   xor()  1418 MB/s
    [    1.389037] raid6: neonx8   gen()  1552 MB/s
    [    1.457054] raid6: neonx8   xor()  1459 MB/s
    [    1.457092] raid6: using algorithm neonx8 gen() 1552 MB/s
    [    1.461047] raid6: .... xor() 1459 MB/s, rmw enabled
    [    1.465978] raid6: using neon recovery algorithm
    [    1.471269] SCSI subsystem initialized
    [    1.474313] libata version 3.00 loaded.
    [    1.474445] usbcore: registered new interface driver usbfs
    [    1.479763] usbcore: registered new interface driver hub
    [    1.485041] usbcore: registered new device driver usb
    [    1.490194] media: Linux media interface: v0.10
    [    1.494547] videodev: Linux video capture interface: v2.00
    [    1.500028] pps_core: LinuxPPS API ver. 1 registered
    [    1.504908] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    1.514002] PTP clock support registered
    [    1.517898] EDAC MC: Ver: 3.0.0
    [    1.521365] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox driver.
    [    1.528670] jesd204: found 0 devices and 0 topologies
    [    1.533318] FPGA manager framework
    [    1.536823] Advanced Linux Sound Architecture Driver Initialized.
    [    1.542978] Bluetooth: Core ver 2.22
    [    1.546273] NET: Registered protocol family 31
    [    1.550672] Bluetooth: HCI device and connection manager initialized
    [    1.556989] Bluetooth: HCI socket layer initialized
    [    1.561831] Bluetooth: L2CAP socket layer initialized
    [    1.566858] Bluetooth: SCO socket layer initialized
    [    1.572168] clocksource: Switched to clocksource arch_sys_counter
    [    1.577914] VFS: Disk quotas dquot_6.6.0
    [    1.581682] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    1.593029] NET: Registered protocol family 2
    [    1.593391] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
    [    1.600691] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
    [    1.607966] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
    [    1.614716] TCP: Hash tables configured (established 32768 bind 32768)
    [    1.620894] UDP hash table entries: 2048 (order: 4, 65536 bytes)
    [    1.626869] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
    [    1.633349] NET: Registered protocol family 1
    [    1.637721] RPC: Registered named UNIX socket transport module.
    [    1.643415] RPC: Registered udp transport module.
    [    1.648092] RPC: Registered tcp transport module.
    [    1.652752] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    1.659430] PCI: CLS 0 bytes, default 64
    [    1.659915] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    1.666391] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
    [    1.674784] Initialise system trusted keyrings
    [    1.678423] workingset: timestamp_bits=62 max_order=20 bucket_order=0
    [    1.685447] NFS: Registering the id_resolver key type
    [    1.689795] Key type id_resolver registered
    [    1.693931] Key type id_legacy registered
    [    1.697916] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    1.704582] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
    [    2.793310] NET: Registered protocol family 38
    [    2.851534] Key type asymmetric registered
    [    2.851572] Asymmetric key parser 'x509' registered
    [    2.854877] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
    [    2.862198] io scheduler noop registered
    [    2.866088] io scheduler deadline registered
    [    2.870346] io scheduler cfq registered (default)
    [    2.874999] io scheduler mq-deadline registered
    [    2.879496] io scheduler kyber registered
    [    2.911211] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
    [    2.915487] cacheinfo: Unable to detect cache hierarchy for CPU 0
    [    2.922450] brd: module loaded
    [    2.926242] loop: module loaded
    [    2.926442] Registered mathworks_ip class
    [    2.928939] mtdoops: mtd device (mtddev=name/number) must be supplied
    [    2.935856] libphy: Fixed MDIO Bus: probed
    [    2.939712] tun: Universal TUN/TAP device driver, 1.6
    [    2.943697] CAN device driver interface
    [    2.948369] usbcore: registered new interface driver asix
    [    2.952796] usbcore: registered new interface driver ax88179_178a
    [    2.958834] usbcore: registered new interface driver cdc_ether
    [    2.964628] usbcore: registered new interface driver net1080
    [    2.970251] usbcore: registered new interface driver cdc_subset
    [    2.976135] usbcore: registered new interface driver zaurus
    [    2.981678] usbcore: registered new interface driver cdc_ncm
    [    2.988001] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    2.993760] ehci-pci: EHCI PCI platform driver
    [    2.998443] usbcore: registered new interface driver uas
    [    3.003480] usbcore: registered new interface driver usb-storage
    [    3.009470] usbcore: registered new interface driver usbserial_generic
    [    3.015923] usbserial: USB Serial support registered for generic
    [    3.021894] usbcore: registered new interface driver ftdi_sio
    [    3.027599] usbserial: USB Serial support registered for FTDI USB Serial Device
    [    3.034872] usbcore: registered new interface driver upd78f0730
    [    3.040748] usbserial: USB Serial support registered for upd78f0730
    [    3.048346] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
    [    3.054202] i2c /dev entries driver
    [    3.059578] usbcore: registered new interface driver uvcvideo
    [    3.063315] USB Video Class driver (1.1.1)
    [    3.068746] Bluetooth: HCI UART driver ver 2.3
    [    3.071784] Bluetooth: HCI UART protocol H4 registered
    [    3.076899] Bluetooth: HCI UART protocol BCSP registered
    [    3.082193] Bluetooth: HCI UART protocol LL registered
    [    3.087274] Bluetooth: HCI UART protocol ATH3K registered
    [    3.092653] Bluetooth: HCI UART protocol Three-wire (H5) registered
    [    3.098905] Bluetooth: HCI UART protocol Intel registered
    [    3.104252] Bluetooth: HCI UART protocol QCA registered
    [    3.109458] usbcore: registered new interface driver bcm203x
    [    3.115070] usbcore: registered new interface driver bpa10x
    [    3.120605] usbcore: registered new interface driver bfusb
    [    3.126057] usbcore: registered new interface driver btusb
    [    3.131480] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
    [    3.137146] usbcore: registered new interface driver ath3k
    [    3.142680] EDAC MC: ECC not enabled
    [    3.146365] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
    [    3.158533] CPUidle arm: Failed to register cpuidle driver
    [    3.163831] sdhci: Secure Digital Host Controller Interface driver
    [    3.169802] sdhci: Copyright(c) Pierre Ossman
    [    3.174127] sdhci-pltfm: SDHCI platform and OF driver helper
    [    3.180151] ledtrig-cpu: registered to indicate activity on CPUs
    [    3.185764] zynqmp_firmware_probe Platform Management API v1.1
    [    3.191518] zynqmp_firmware_probe Trustzone version v1.0
    [    3.199564] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
    [    3.226990] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22
    [    3.229702] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
    [    3.234812] zynqmp_aes zynqmp_aes: AES Successfully Registered

    [    3.242332] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
    [    3.248462] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [    3.254095] usbcore: registered new interface driver usbhid
    [    3.259368] usbhid: USB HID core driver
    [    3.269801] axi_sysid 85000000.axi-sysid-0: [adrv9001] [CMOS_LVDS_N=0] on [zcu102] git <19f7a0b279c28d13e7f8836842f4cd2040594253> clean [2021-01-19 12:53:35] UTC
    [    3.278899] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
    [    3.285479] usbcore: registered new interface driver snd-usb-audio
    [    3.292904] pktgen: Packet Generator for packet performance testing. Version: 2.75
    [    3.299007] Initializing XFRM netlink socket
    [    3.302943] NET: Registered protocol family 10
    [    3.307636] Segment Routing with IPv6
    [    3.311004] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    3.317133] NET: Registered protocol family 17
    [    3.321230] NET: Registered protocol family 15
    [    3.325634] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
    [    3.338720] can: controller area network core (rev 20170425 abi 9)
    [    3.344747] NET: Registered protocol family 29
    [    3.349069] can: raw protocol (rev 20170425)
    [    3.353304] can: broadcast manager protocol (rev 20170425 t)
    [    3.358930] can: netlink gateway (rev 20170425) max_hops=1
    [    3.364487] Bluetooth: RFCOMM TTY layer initialized
    [    3.369228] Bluetooth: RFCOMM socket layer initialized
    [    3.374347] Bluetooth: RFCOMM ver 1.11
    [    3.378084] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    3.383323] Bluetooth: BNEP filters: protocol multicast
    [    3.388516] Bluetooth: BNEP socket layer initialized
    [    3.393444] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    3.399328] Bluetooth: HIDP socket layer initialized
    [    3.404361] 9pnet: Installing 9P2000 support
    [    3.408506] NET: Registered protocol family 36
    [    3.412923] Key type dns_resolver registered
    [    3.417651] registered taskstats version 1
    [    3.421223] Loading compiled-in X.509 certificates
    [    3.426303] Btrfs loaded, crc32c=crc32c-generic
    [    3.436877] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
    [    3.446196] console [ttyPS0] enabled
    [    3.449796] bootconsole [cdns0] disabled
    [    3.457857] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps
    [    3.471237] of-fpga-region fpga-full: FPGA Region probed
    [    3.477060] nwl-pcie fd0e0000.pcie: Link is DOWN
    [    3.481703] nwl-pcie fd0e0000.pcie: host bridge /amba/pcie@fd0e0000 ranges:
    [    3.488674] nwl-pcie fd0e0000.pcie:   MEM 0xe0000000..0xefffffff -> 0xe0000000
    [    3.495896] nwl-pcie fd0e0000.pcie:   MEM 0x600000000..0x7ffffffff -> 0x600000000
    [    3.503476] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
    [    3.509652] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    3.515135] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
    [    3.522004] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
    [    3.529503] pci 0000:00:00.0: [10ee:d021] type 01 class 0x060400
    [    3.529559] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
    [    3.534095] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
    [    3.540223] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
    [    3.546797] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
    [    3.553906] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
    [    3.561017] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
    [    3.568121] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
    [    3.575227] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
    [    3.582335] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
    [    3.589444] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
    [    3.596546] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
    [    3.603804] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
    [    3.615171] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13
    [    3.623843] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
    [    3.634625] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
    [    3.642724] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
    [    3.651207] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
    [    3.663644] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
    [    3.676317] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
    [    3.686502] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
    [    3.693520] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    3.700130] [drm] No driver support for vblank timestamp query.
    [    3.706109] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008dc2e70)
    [    3.861290] Console: switching to colour frame buffer device 160x50
    [    3.884256] zynqmp-display fd4a0000.zynqmp-display: fb0:  frame buffer device
    [    3.891584] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
    [    3.899692] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
    [    3.908733] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
    [    3.916614] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
    [    3.925574] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
    [    3.936226] scsi host0: ahci-ceva
    [    3.939769] scsi host1: ahci-ceva
    [    3.943222] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37
    [    3.951136] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37
    [    3.960573] m25p80 spi0.0: SPI-NOR-UniqueID 1044001821860015010006009ff89e784d
    [    3.967795] m25p80 spi0.0: found n25q512a, expected m25p80
    [    3.973540] m25p80 spi0.0: n25q512a (131072 Kbytes)
    [    3.978437] 4 fixed-partitions partitions found on MTD device spi0.0
    [    3.984785] Creating 4 MTD partitions on "spi0.0":
    [    3.989572] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
    [    3.995781] 0x000000100000-0x000000600000 : "qspi-linux"
    [    4.001484] 0x000000600000-0x000000620000 : "qspi-device-tree"
    [    4.007703] 0x000000620000-0x000000c00000 : "qspi-rootfs"
    [    4.015547] macb ff0e0000.ethernet: Not enabling partial store and forward
    [    4.022911] libphy: MACB_mii_bus: probed
    [    4.026907] mdio_bus ff0e0000.ethernet-ffffffff: MDIO device at address 21 is missing.
    [    4.037088] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
    [    4.050126] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 22 (9e:43:a0:07:0e:c4)
    [    4.060268] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
    [    4.066807] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
    [    4.073302] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
    [    4.079803] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
    [    4.087626] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
    [    4.093543] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
    [    4.101790] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    4.107285] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
    [    4.115833] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000202010810
    [    4.125239] xhci-hcd xhci-hcd.0.auto: irq 48, io mem 0xfe200000
    [    4.131362] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [    4.139623] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.146845] usb usb1: Product: xHCI Host Controller
    [    4.151720] usb usb1: Manufacturer: Linux 4.19.0-g11b5080 xhci-hcd
    [    4.157890] usb usb1: SerialNumber: xhci-hcd.0.auto
    [    4.163039] hub 1-0:1.0: USB hub found
    [    4.166811] hub 1-0:1.0: 1 port detected
    [    4.170918] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
    [    4.176410] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
    [    4.184063] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0  SuperSpeed
    [    4.190783] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
    [    4.199043] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    4.206266] usb usb2: Product: xHCI Host Controller
    [    4.211139] usb usb2: Manufacturer: Linux 4.19.0-g11b5080 xhci-hcd
    [    4.217312] usb usb2: SerialNumber: xhci-hcd.0.auto
    [    4.222427] hub 2-0:1.0: USB hub found
    [    4.226187] hub 2-0:1.0: 1 port detected
    [    4.231357] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
    [    4.238605] pca953x 0-0020: Linked as a consumer to regulator.0
    [    4.245394] GPIO line 496 (sel0) hogged as output/low
    [    4.250775] GPIO line 497 (sel1) hogged as output/high
    [    4.256244] GPIO line 498 (sel2) hogged as output/high
    [    4.261714] GPIO line 499 (sel3) hogged as output/high
    [    4.267047] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
    [    4.269302] ata2: SATA link down (SStatus 0 SControl 330)
    [    4.274299] pca953x 0-0021: Linked as a consumer to regulator.0
    [    4.279674] ata1: SATA link down (SStatus 0 SControl 330)
    [    4.287069] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.297761] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.304590] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.311405] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.318216] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.325027] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.331843] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.338660] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.345477] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.352292] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.358701] i2c i2c-0: Added multiplexed i2c bus 3
    [    4.364186] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
    [    4.370993] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.377753] random: fast init done
    [    4.377815] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.387950] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.395295] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.402115] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.408935] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.415751] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
    [    4.422164] i2c i2c-0: Added multiplexed i2c bus 4
    [    4.462084] i2c i2c-0: Added multiplexed i2c bus 5
    [    4.467050] i2c i2c-0: Added multiplexed i2c bus 6
    [    4.471840] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
    [    4.479189] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 24
    [    4.487012] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
    [    4.493763] i2c i2c-1: Added multiplexed i2c bus 7
    [    4.498897] i2c i2c-1: Added multiplexed i2c bus 8
    [    4.505804] si570 9-005d: registered, current frequency 300000000 Hz
    [    4.512205] i2c i2c-1: Added multiplexed i2c bus 9
    [    4.520182] usb 1-1: new full-speed USB device number 2 using xhci-hcd
    [    4.530998] si570 10-005d: registered, current frequency 148500000 Hz
    [    4.537488] i2c i2c-1: Added multiplexed i2c bus 10
    [    4.542582] si5324 11-0069: si5328 probed
    [    4.604236] si5324 11-0069: si5328 probe successful
    [    4.609157] i2c i2c-1: Added multiplexed i2c bus 11
    [    4.614197] i2c i2c-1: Added multiplexed i2c bus 12
    [    4.619236] i2c i2c-1: Added multiplexed i2c bus 13
    [    4.624277] i2c i2c-1: Added multiplexed i2c bus 14
    [    4.629154] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
    [    4.637115] i2c i2c-1: Added multiplexed i2c bus 15
    [    4.668858] i2c i2c-1: Added multiplexed i2c bus 16
    [    4.673925] i2c i2c-1: Added multiplexed i2c bus 17
    [    4.678985] i2c i2c-1: Added multiplexed i2c bus 18
    [    4.684039] i2c i2c-1: Added multiplexed i2c bus 19
    [    4.689092] i2c i2c-1: Added multiplexed i2c bus 20
    [    4.694152] i2c i2c-1: Added multiplexed i2c bus 21
    [    4.699209] i2c i2c-1: Added multiplexed i2c bus 22
    [    4.704086] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
    [    4.711691] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 25
    [    4.718108] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
    [    4.727241] usb 1-1: New USB device found, idVendor=05e3, idProduct=0606, bcdDevice= 7.02
    [    4.735418] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
    [    4.742548] usb 1-1: Product: USB Hub 2.0
    [    4.746549] usb 1-1: Manufacturer: ALCOR
    [    4.781246] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
    [    4.913179] mmc0: new ultra high speed SDR104 SDHC card at address aaaa
    [    4.920283] mmcblk0: mmc0:aaaa SC32G 29.7 GiB
    [    4.929029]  mmcblk0: p1 p2 p3
    [    4.959044] hub 1-1:1.0: USB hub found
    [    4.962904] hub 1-1:1.0: 4 ports detected
    [    5.252174] usb 1-1.3: new low-speed USB device number 3 using xhci-hcd
    [    5.371110] usb 1-1.3: New USB device found, idVendor=03f0, idProduct=0024, bcdDevice= 3.00
    [    5.379458] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=0
    [    5.386766] usb 1-1.3: Product: HP Basic USB Keyboard
    [    5.391808] usb 1-1.3: Manufacturer: CHICONY
    [    5.605818] input: CHICONY HP Basic USB Keyboard as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1.3/1-1.3:1.0/0003:03F0:0024.0001/input/input0
    [    5.680438] hid-generic 0003:03F0:0024.0001: input: USB HID v1.10 Keyboard [CHICONY HP Basic USB Keyboard] on usb-xhci-hcd.0.auto-1.3/input0
    [    5.772173] usb 1-1.4: new low-speed USB device number 4 using xhci-hcd
    [    5.911548] usb 1-1.4: New USB device found, idVendor=045e, idProduct=0040, bcdDevice= 3.00
    [    5.919894] usb 1-1.4: New USB device strings: Mfr=1, Product=3, SerialNumber=0
    [    5.927202] usb 1-1.4: Product: Microsoft 3-Button Mouse with IntelliEye(TM)
    [    5.934240] usb 1-1.4: Manufacturer: Microsoft
    [    6.113348] input: Microsoft Microsoft 3-Button Mouse with IntelliEye(TM) as /devices/platform/amba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1.4/1-1.4:1.0/0003:045E:0040.0002/input/input1
    [    6.131331] hid-generic 0003:045E:0040.0002: input: USB HID v1.10 Mouse [Microsoft Microsoft 3-Button Mouse with IntelliEye(TM)] on usb-xhci-hcd.0.auto-1.4/input0
    [    7.432532] random: crng init done
    [   11.555337] adrv9002 spi1.0: adrv9002-phy Rev 11.0, Firmware 0.12.2.13,  Stream 0.5.6.0,  API version: 29.2.0 successfully initialized
    [   12.182658] cf_axi_adc 84a00000.axi-adrv9002-rx-lpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0x00000000af6b9ae1, probed ADC ADRV9002 as MASTER
    [   12.196023] cf_axi_tdd 84a0c800.axi-adrv9002-core-tdd-lpc: Major version mismatch between PCORE and driver. Driver expected 1.00.a, PCORE reported 173.222.\xad
    [   12.228577] cf_axi_dds 84a02000.axi-adrv9002-tx-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A02000 mapped to 0x000000009bce400f, probed DDS ADRV9002
    [   12.245520] input: gpio-keys as /devices/platform/gpio-keys/input/input2
    [   12.252483] rtc_zynqmp ffa60000.rtc: setting system clock to 2021-03-03 07:41:20 UTC (1614757280)
    [   12.261356] of_cfs_init
    [   12.263810] of_cfs_init: OK
    [   12.266730] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [   12.405641] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [   12.412231] zynqmp_pll_disable() clock disable failed for dpll_int, ret = -13
    [   12.420053] ALSA device list:
    [   12.423014]   #0: DisplayPort monitor
    [   12.427022] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    [   12.435633] cfg80211: failed to load regulatory.db
    [   12.525333] EXT4-fs (mmcblk0p2): recovery complete
    [   12.530778] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [   12.538890] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [   12.548352] devtmpfs: mounted
    [   12.551498] Freeing unused kernel memory: 832K
    [   12.555976] Run /sbin/init as init process
    [   12.797567] systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
    [   12.819316] systemd[1]: Detected architecture arm64.
    [   12.838753] systemd[1]: Set hostname to <analog>.
    [   12.989227] systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
    [   13.006276] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    [   13.263620] systemd[1]: Listening on udev Kernel Socket.
    [   13.284500] systemd[1]: Listening on udev Control Socket.
    [   13.304505] systemd[1]: Listening on Journal Socket (/dev/log).
    [   13.328603] systemd[1]: Created slice User and Session Slice.
    [   13.348488] systemd[1]: Listening on Journal Socket.
    [   14.019000] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [   14.216767] systemd-journald[2677]: Received request to flush runtime journal from PID 1
    [   19.395645] pps pps0: new PPS source ptp0
    [   19.395657] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered.
    [   19.395758] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [   19.485607] Adding 102396k swap on /var/swap.  Priority:-2 extents:1 across:102396k SS
    [   20.404800] macb ff0e0000.ethernet eth0: link up (1000/Full)
    [   20.404822] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [ 2598.543644] adrv9002 spi1.0: [ERROR]: Error number  6 (0x00000006), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_StartStatus_Check, in line  161, variable name NULL.Error message Bootup clkgen setup error.
    [ 2598.543652] adrv9002 spi1.0: adrv9002_digital_init, 2083: failed with "Bootup clkgen setup error" (6)
    [ 2599.660746] adrv9002 spi1.0: [ERROR]: Error number  6 (0x00000006), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_StartStatus_Check, in line  161, variable name NULL.Error message Bootup clkgen setup error.
    [ 2599.660753] adrv9002 spi1.0: adrv9002_digital_init, 2083: failed with "Bootup clkgen setup error" (6)
    [ 2599.661023] adrv9002 spi1.0: [ERROR]: Error number  4098 (0x00001002), Recovery action -104.In file drivers/iio/adc/navassa/devices/adrv9001/private/src/adrv9001_gpio.c, in function adrv9001_GpIntHandler, in line  225, variable name gpIntStatus->gpIntStatus.Error message Unknown GP Interrupt source.
    [ 2599.661033] adrv9002 spi1.0: [ERROR]: Error number  4098 (0x00001002), Recovery action -104.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_gpio.c, in function adi_adrv9001_gpio_GpIntHandler, in line  76, variable name NULL.Error message Unknown GP Interrupt source.
    [ 2599.661038] adrv9002 spi1.0: GP Interrupt Status 0x06000000 Mask 0x0E00E0F0
    [ 2599.661272] adrv9002 spi1.0: [ERROR]: Error number  4098 (0x00001002), Recovery action -104.In file drivers/iio/adc/navassa/devices/adrv9001/private/src/adrv9001_gpio.c, in function adrv9001_GpIntHandler, in line  225, variable name gpIntStatus->gpIntStatus.Error message Unknown GP Interrupt source.
    [ 2599.661281] adrv9002 spi1.0: [ERROR]: Error number  4098 (0x00001002), Recovery action -104.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_gpio.c, in function adi_adrv9001_gpio_GpIntHandler, in line  76, variable name NULL.Error message Unknown GP Interrupt source.
    [ 2599.661286] adrv9002 spi1.0: GP Interrupt Status 0x00000000 Mask 0x0000E0F0

  • 0
    •  Analog Employees 
    on Mar 3, 2021 6:46 PM in reply to kozlova

    What model is on the white product sticker?

    -Travis

  • On the front:

    ADRV9002

    NP/W1=0.03-3GHz

    on the back:

    S20-0719

    SN:00116