ADRV9009+KCU706 Python code

Hi everyone,

hope you're doing well. Juste wondering if the is an example of python code to configure the Tx/Rx of the ADRV9009+KCU706.

I follows some example on the website :https://analogdevicesinc.github.io/pyadi-iio/devices/adi.adrv9009.html

but some command return error : like setting the sampling frequency or the RF bandwith.

sdr.tx_rf_bandwidth = 200e6 # (100 MHz => 122.88MHz 200MHz =>245.76)
AttributeError: can't set attribute

sdr.tx_sample_rate = 245.76e6
AttributeError: can't set attribute

Also when i set the Rx/Tx_lo, nothing appends.

Kind regards!

E.K