gr-iio-ad9371

Hello , I  am using AD9371and ZC706 board. I have installed GNU radio and gr-iio-ad9371 branch to my Ubuntu16.04.and I have installed in  /home/usg/gnuradio/gr-iio-ad9371/gr-iio/

I have a problem that GRC is not connecting to the ZC706 board. I am making the files my Ubuntu host PC(VM ware). 

Ping to the board gives me communication.

PING 192.168.1.2 (192.168.1.2) 56(84) bytes of data.
64 bytes from 192.168.1.2: icmp_seq=1 ttl=128 time=0.608 ms
64 bytes from 192.168.1.2: icmp_seq=2 ttl=128 time=0.632 ms

I am using one of the example projects to run. And it gives me an error when "execute the flow graph".

Executing: /usr/bin/python -u /home/usg/gnuradio/gr-iio-ad9371/gr-iio/iio-examples/top_block.py

Using Volk machine: avx2_64_mmx_orc
ERROR: Unable to find host: Name or service not known

In my FMComms properties URI is configured as "uri" and shows in the blocks ":ip...local"

How can I correct this ? Why the board is not connecting ?

I have referred https://ez.analog.com/sw-interface-tools/f/q-a/164522/boot-adrv9361-z7035-board/372760#372760

Parents Reply Children