Trouble setting up AD9837 correctly

I am trying to use a TI MSP432 to generate a square wave signal from an AD9837 (more specifically, a SparkFun Minigen that uses the AD9837). The control register seems to be straightforward, but I can't figure out why the board is not producing the correct output signal. 

 The code that controls the AD9837 is here:

#include <ti/devices/msp432p4xx/driverlib/driverlib.h>
#include <ti/drivers/GPIO.h>
#include <ti/drivers/SPI.h>
#include "minigen.h"

int n;

void minigen_reset(){
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
uint32_t defaultFreq = minigen_freqCalc(100.0);
minigen_adjustFreq(FREQ0, FULL, defaultFreq);
minigen_adjustFreq(FREQ1, FULL, defaultFreq);
minigen_adjustPhaseShift(PHASE0, 0x0000);
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
SPI_transmitData(EUSCI_B0_BASE, 0x01);
SPI_transmitData(EUSCI_B0_BASE, 0x00);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
SPI_transmitData(EUSCI_B0_BASE, 0x00);
SPI_transmitData(EUSCI_B0_BASE, 0x00);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}

// Set the mode of the part. The mode (trinagle, sine, or square) is set by
// three bits in the status register: D5 (OPBITEN), D3 (DIV2), and D1 (MODE).
// Here's a nice truth table for those settings:
// D5 D1 D3
// 0 0 x Sine wave output
// 0 1 x Triangle wave output
// 1 0 0 Square wave @ 1/2 frequency
// 1 0 1 Square wave @ frequency
// 1 1 x Not allowed
void minigen_setMode(MODE newMode){
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
// We want to adjust the three bits in the config register that we're
// interested in without screwing up anything else. Unfortunately, this
// part is write-only, so we need to maintain a local shadow, adjust that,
// then write it.
configReg &= ~0x002A; // Clear D5, D3, and D1.
// This switch statement sets the appropriate bit in the config register.
switch(newMode)
{
case TRIANGLE:
configReg |= 0x0002;
break;
case SQUARE_2:
configReg |=0x0020;
break;
case SQUARE:
configReg |=0x0028;
break;
case SINE:
configReg |=0x0000;
break;
}
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n < 2; n++)
SPI_transmitData(EUSCI_B0_BASE, (configReg >> (8*n)) & 0xFF); // Now write our shadow copy to the part.
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}

// The AD9837 has two frequency registers that can be independently adjusted.
// This allows us to fiddle with the value in one without affecting the output
// of the device. The register used for calculating the output is selected by
// toggling bit 11 of the config register.
void minigen_selectFreqReg(FREQREG reg)
{
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
// For register FREQ0, we want to clear bit 11.
if (reg == FREQ0) configReg &= ~0x0800;
// Otherwise, set bit 11.
else configReg |= 0x0800;
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n <= 1; n++)
SPI_transmitData(EUSCI_B0_BASE, (configReg >> (8*n)) & 0xFF);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}


// Similarly, there are two phase registers, selected by bit 10 of the config
// register.
void minigen_selectPhaseReg(PHASEREG reg)
{
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
if (reg == PHASE0) configReg &= ~0x0400;
else configReg |= 0x0400;
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n <= 1; n++)
SPI_transmitData(EUSCI_B0_BASE, (configReg >> (8*n)) & 0xFF);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}


// The frequency registers are 28 bits in size (combining the lower 14 bits of
// two 16 bit writes; the upper 2 bits are the register address to write).
// Bits 13 and 12 of the config register select how these writes are handled:
// 13 12
// 0 0 Any write to a frequency register is treated as a write to the lower
// 14 bits; this allows for fast fine adjustment.
// 0 1 Writes are send to upper 14 bits, allowing for fast coarse adjust.
// 1 x First write of a pair goes to LSBs, second to MSBs. Note that the
// user must, in this case, be certain to write in pairs, to avoid
// unexpected results!
void minigen_setFreqAdjustMode(FREQADJUSTMODE newMode)
{
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
// Start by clearing the bits in question.
configReg &= ~0x3000;
// Now, adjust the bits to match the truth table above.
switch(newMode)
{
case COARSE: // D13:12 = 01
configReg |= 0x1000;
break;
case FINE: // D13:12 = 00
break;
case FULL: // D13:12 = 1x (we use 10)
configReg |= 0x2000;
break;
}
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n <= 1; n++)
SPI_transmitData(EUSCI_B0_BASE, (configReg >> (8*n)) & 0xFF);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}

// The phase shift value is 12 bits long; it gets routed to the proper phase
// register based on the value of the 3 MSBs (4th MSB is ignored).
void minigen_adjustPhaseShift(PHASEREG reg, uint16_t newPhase)
{
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
// First, let's blank the top four bits. Just because it's the right thing
// to do, you know?
newPhase &= ~0xF000;
// Now, we need to set the top three bits to properly route the data.
// D15:D13 = 110 for PHASE0...
if (reg == PHASE0) newPhase |= 0xC000;
// ... and D15:D13 = 111 for PHASE1.
else newPhase |= 0xE000;
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n <= 1; n++)
SPI_transmitData(EUSCI_B0_BASE, (configReg >> (8*n)) & 0xFF);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}

// Okay, now we're going to handle frequency adjustments. This is a little
// trickier than a phase adjust, because in addition to properly routing the
// data, we need to know whether we're writing all 32 bits or just 16. I've
// overloaded this function call for three cases: write with a mode change (if
// one is needed), and write with the existing mode.

// Adjust the contents of the given register, and, if necessary, switch mode
// to do so. This is probably the slowest method of updating a register.
void minigen_adjustFreq(FREQREG reg, FREQADJUSTMODE mode, uint32_t newFreq)
{
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
minigen_setFreqAdjustMode(mode);

// We need to split the 32-bit input into two 16-bit values, blank the top
// two bits of those values, and set the top two bits according to the
// value of reg.
// Start by acquiring the low 16-bits...
uint16_t temp = (uint16_t)newFreq;
// ...and blanking the first two bits.
temp &= ~0xC000;
// Now, set the top two bits according to the reg parameter.
if (reg==FREQ0) temp |= 0x4000;
else temp |= 0x8000;
// Now, we can write temp out to the device.
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n <= 1; n++)
SPI_transmitData(EUSCI_B0_BASE, (temp >> (8*n)) & 0xff);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
// Okay, that's the lower 14 bits. Now let's grab the upper 14.
temp = (uint16_t)(newFreq>>14);
// ...and now, we can just repeat the process.
temp &= ~0xC000;
// Now, set the top two bits according to the reg parameter.
if (reg==FREQ0) temp |= 0x4000;
else temp |= 0x8000;
// Now, we can write temp out to the device.
GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
for (n = 0; n <= 1; n++)
SPI_transmitData(EUSCI_B0_BASE, (temp >> (8*n)) & 0xff);
GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN0);
}

// Helper function, used to calculate the integer value to be written to a
// freq register for a desired output frequency.
// The output frequency is fclk/2^28 * FREQREG. For us, fclk is 16MHz. We can
// save processor time by specifying a constant for fclk/2^28- .0596. That is,
// in Hz, the smallest step size for adjusting the output frequency.
uint32_t minigen_freqCalc(float desiredFrequency)
{
return (uint32_t) (desiredFrequency/.0596);
}

Sorry if this is formatted badly - I'm having trouble figuring out these forum tools!


Since the MSP432 can only send one byte at a time with the SPI_transmitData, I am not sure if I am sending the control bits correctly. Also, I am using Pin 3.0 (with the GPIO) as the FSYNC to the board. Am I using this logic correctly to set the FSYNC low when I want to transmit data?

Please let me know if I can approve this post to make my question more clear. Thank you in advance for your help!

Parents Reply Children
No Data