Post Go back to editing

AD734 as a Lock in amplifier noise spikes

Category: Hardware
Product Number: AD734

Hello,

I’m trying to use the AD734 as a ‘Lock in’ amplifier.

I have the AD734 on a breadboard connected as in fig. 24 page 20 of the datasheet (basic multiplier circuit).

The denominator is set to 1V with the resistors specified in table 5 page 20 of the datasheet.

X1 input is a sine wave with an amplitude of 300mV (600mV p-p) and a frequency of 350 KHz.

X2 is grounded.

Y1 input is a square wave with an amplitude of 1V (2V p-p) and the frequency of 350 KHz.

Y2 is grounded.

At the output I have a the fully rectified sine wave but small spikes appears (FIG. 1 below) at half the frequency  (350KHz /2).

fig.1

If the amplitude of the square wave is increased to just 3V p-p the spikes exponentially increases (fig.2 and 3).

fig.2

fig.3

I can’t get rid of them.

Any suggestion?

Thanks