Post Go back to editing

AD9434 non FMC board compatibility with AD-ADC-FMC to integrate it with ZEDBOARD

Hi,

    I am new to the FPGA working on the project which require collection of analog data using ADC AD9434 and send it to Zedboard Zynq 7000. the problem is that the ADC that I received is :"AD9434-500EBZ" instead of "AD9434-FMC-500EBZ" i.e. without the FMC connector which makes it unable to connect to the zedboard. I was thinking of using an AD-ADC-FMC board to make it work. I need some guidance in that regards.