ADALM2000 Spectrum Analyzer

I'm not seeing anything on the spectrum analyzer for either channel.  My circuit is a two stage op amp.  My input frequency is a 1kHz sine wave with 200mV peak.  I can measure the input and output of the circuit very well with the Oscope for Channel 1 and Channel 2.  My gain is about 3.2V/V.  Channel 1 is the input and Channel 2 is the output.

Can anyone suggest what I might be doing wrong?  The read the instructions on the wiki site for the spectrum analyzer but nothing seemed apparent of what i am doing wrong.

Thanks!