I could not find a way to adjust the vertical axis on the Network Analyzer app itself. The Analyzer page seems quite out of date. Since it is now different than the web page that was no help. Is it possible to adjust the V scale and I am just missing it or is there no way to adjust (directly or indirectly) the vertical axis scaling? I'm measuring a simple RLC network with a Q greater than 6. This causes the gain to be greater than 3dB. The plot values are still available. You just can't see them as they get clipped in the plot.
Mark Allie