Question 1:
In figure 5 the maximum power of a solar cell is given. Which physical size does have an influence?
Answer:
Of course, the light intensity has an influence on the maximum power of a solar cell.
Question 2:
What is the maximum power you could get out of the solar cell?
Answer:
Please see figure 6. The power maximum at the given light conditions is about 19.5mW.
Question 3:
How is the function called to keep the output Power at the maximum level? (Tip see ADP5091)
Answer:
MPPT – Maximum power point tracking
This function ensures you are getting always the maximum possible power out of a solar cell. The maximum power might be different based on the light conditions - MPPT ensures it will be always at the maximum possible.